Tool/software:
Hello Support-Team,
I am sorry, but missed the window to reply to the original thread, so I will try to continue here.
From Nihil Dasan:
Hi Marco,
No, if the memory map is unchanged, then there need not be any changes in this file
Then let us focus on this error
[C7x_2 ] 15.527368 s: VX_ZONE_ERROR:[ownTargetCmdDescHandler:1115] object descriptor type is invalidIs this the first error that you are seeing or are there any others present above this?
Can you share the full logs?
Yes, this is the first error that is encountered, but it does not do so deterministically.
Usually the test run just stops after
[ RUN 0001 ] tivxTestKernelsNotNot.Sizes/0/640x480 ...
Only from time to time I get the error message.
I will attach the full logs.
Thanks and kind regards,
Marco