This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am working with the AM6442 Sitara Processor from Texas Instruments, which features an ARM Cortex-A53 core running Linux and ARM Cortex-R5F cores running bare-metal code. I am trying to implement mailbox-based communication between the A53 core (running Linux) and the R5F cores (running bare-metal).
Here are my specific questions:
1) How do I set up the mailbox driver on the A53 core running Linux?
2) How can I configure the R5F cores (bare-metal) to handle messages from the A53 core?
3)How are interrupts handled in the context of mailbox communication? What are the best practices for synchronizing message passing between the A53 and R5F cores?
4) Are there any example codes or application notes that show how to implement this kind of mailbox messaging between the A53 and R5F cores on the AM6442?
Hi Kiran, any particular reason you need to create your own A53 + R5F mailbox communication? Or, can IPC (which uses underlining HW Mailboxes) being used?
Some links as a reference below:
Welcome to the Multicore Academy module!
Thank you,
Paula