This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I need to confirm that we are allowed to swap data bits within a given data byte lane on the DM3730 to assist on breakout. (ie swapping d0 with d7). Additionally are we also allowed to swap entire bytes for example (d7:0 & dm0 & dqs0) with (d15:9 & dmn1 & dqs1)?
Thank you
Paul,
Neither the memory nor the EMIF will care if two or eight pins are swapped just so long as they are in the same byte lane. Just be certain to follow the DDR layout guidelines in section 6.4.2 of the datasheet.