Tool/software:
Hi TI Expert,
I need confirmations related to this SERDES allocation/configuration and QSGMII application restriction:
SPRUJ52C Table 12-198. SERDES0/1/2/4 Supported Configurations

Will it be possible to do this configuration to use all SERDES link, at his full capability ?
SERDES0: 1x4L of PCIE1
SERDES1:
Lane0 SGMII3
Lane1 SGMII4
Lane2 PCIE2 Lane0
Lane3 PCIE2 Lane1
SERDES2:
Lane0 QSGMII5 or SGMII5
Lane1 NA
Lane2 USXGMII on SGMII1 (10Gbps)
Lane3 USXGMII on SGMII2 (10Gbps)
Especially the full capability of the 2 USXGMII Links on the same SERDES Block ?
Could you confirm that this configuration, the QSGMII link will not trouble the other link ?
In regards with this information, taken from :
SPRSP79B Table 4-1. Device Comparison Remark7
If QSGMII is used on any SGMII Port 1 thru 4, then SGMII1/2/3/4 cannot be used for Ethernet functionality since all 4 internal CPSW
ports map to the selected QSGMII SERDES port.
If QSGMII is used on any SGMII Port 5 thru 8, then SGMII5/6/7/8 cannot be used for Ethernet functionality since all 4 internal CPSW
ports map to the selected QSGMII SERDES port.
Regards,
AB