This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: mcu+ build errors for sbl

Part Number: AM625


Tool/software:

Hello,

I'm compiling the SBL examples on windows and I'm running into a similar issue as the referenced post where it looks like the makefile can't find some object files to link the sbl together:

 Linking: am62x:r5fss0-0:nortos:ti-arm-clang sbl_emmc_linux_stage1.release.out ...
tiarmclang: error: no such file or directory: 'obj/release/ti_drivers_config.obj'
tiarmclang: error: no such file or directory: 'obj/release/ti_drivers_open_close.obj'
tiarmclang: error: no such file or directory: 'obj/release/ti_board_config.obj'
tiarmclang: error: no such file or directory: 'obj/release/ti_board_open_close.obj'
tiarmclang: error: no such file or directory: 'obj/release/ti_dpl_config.obj'
tiarmclang: error: no such file or directory: 'obj/release/ti_pinmux_config.obj'
tiarmclang: error: no such file or directory: 'obj/release/ti_power_clock_config.obj'
make[2]: *** [sbl_emmc_linux_stage1.release.out] Error 1
make[1]: *** [sbl] Error 2
make: *** [sbl] Error 2

I'm on the latest 10.01 MCU plus SDK for AM62 and have installed the dependencies described in the getting started guide. I also tried to specifically build the sbl stage 2 that the python flash loader script requires for the AM62-SK, but that build also fails.

How do you resolve this build error?

Munan