This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hey everyone,
I am an electronics engineer working on fine-tuning the CPU board of our design, where we are integrating a SoC AM6422 and two TI DP83869 Ethernet PHYs, following the configuration below:
We are aiming to optimize the RGMII timings between the AM64 and our Ethernet PHYs, and we are relying on the TI application note SNLA243 to guide our adjustments.
We have conducted a series of tests to understand and adjust the transmission and reception delays, and we would like to validate our analysis with you before finalizing our configuration.
The goal of this fine-tuning is to correctly adjust the RX and TX delays in RGMII to ensure robust communication and proper clock edge positioning relative to the data signals.
We have observed that:
We have conducted several detailed tests (outlined below) to analyze these phenomena.
️ Tests and Observations
RX Adjustment and Validation
By adjusting the rx-internal-delay-ps in the Device Tree, we were able to center the RXC edges within the data eye.
Below is the measurement of RXC and RX_Dx, where the least dense curve represents no delay (0x00) and the densest curve represents a delay (0x77):
This measurement allowed us to observe in real time that we can indeed influence RX timing.
After adjusting the delay via register settings, we obtained the following curves:
The communication is stable, with edges positioned slightly more within the open part of the eye (white dashed lines), and the setup/hold margins appear to be correct.
From our perspective, this configuration is functional and validated.
️ Tests and Anomalies in TX
The initial configuration in the Device Tree was:
tx-internal-delay-ps = <250>;
rx-internal-delay-ps = <2000>;
As it stands, communication works well, and iperf (a network performance measurement tool that tests bandwidth, throughput, and latency between two hosts) runs correctly.
We modified the TX_DELAY values via the Device Tree and PHY registers (e.g., register 0x86), but observed no visible effect on the TX signals.
From the TX eye diagram, the situation seems borderline:
The clock edges align with the most open part of the eye, but they are too close to the TX_D transitions, approaching setup/hold constraint limits. Ideally, we would like to shift these edges to the left to recenter the timing (which would be like “moving back in time” by adjusting TXC).
Degraded Tests: How We “Broke” the Communication
To better understand the impact of the settings, we intentionally attempted to disrupt communication by modifying certain parameters:
This leads us to question whether some settings are effectively considered and what the exact cause of this communication loss might be.
What We Believe We Have Understood
EDIT: Based on the first feedback we had from TI FAE, we understand that TX delay is an internal delay block that does not manifest physically in measurements. Instead, it impacts the internal timing relationship between the PHY die and its pins.
Updated Questions for TI
Thank you in advance for your help and insights!
Jamel
The AM64x device does not support tuning of its output signals. There is a reserved register bit associated with the AM64x MAC that allows the data to be launched at the same time as the clock transition, or allows the data to be launched 1/4 cycle ahead of the clock transition. This register bit defaults to the state that introduces the internal delay on clock because the AM64x device does not support the first option. The AM64x device was not timing closed to use the first option. Therefore, you should be seeing a fixed delay relationship when observing the TX data path. I think the tuning you are doing is associated with the RGMII PHY. If so, I would expect the see a change in the RX data path, but not the TX data path because the TX delay you are introducing is internal to the RGMII PHY.
Regards,
Paul
Does your PCB design introducing significantly more delay on the TX clock relative to TX data? I ask because I would have expected the delay relationship to be different than what is shown in the snapshot provided. Did you deskew your scope probes to make sure one is not introducing more delay than the other?
Regards,
Paul
Our PCB traces are less than 10 cm long, and we have implemented length matching to ensure proper signal integrity. This should minimize the impact of PCB propagation delays. However, after checking scope probes, it looks like our initial measurements may have been skewed by a 1.34 ns probe delay, which could have misled our interpretation of the TXC vs. TX_Dx timing. Given this, we’re planning to redo our measurements properly to confirm the actual timing relationship. We appreciate your guidance, it really helped us clarify the situation. We'll update once we have more accurate data!