Part Number: PROCESSOR-SDK-J784S4
Tool/software:
Hi,
We have identified a section in the TRM that mentions the SerDES can be configured in loopback mode: "Serial bit stream and parallel word loopback for both line and parallel side."
We need confirmation on the following:
1. If `CSL_SERDES_LOOPBACK_SER` is used to enable loopback, does it simulate the connection of the TX differential pair to the RX?
2. Does `CSL_SERDES_LOOPBACK_LINE` behave as if the input and output are connected on the peripheral side?
Thank you.
Best regards,
Romain