This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Affinity of encoder input and PRU

Part Number: AM6442

Tool/software:

Hi experts,

Sorry for this basic question.

Does the AM64x support the following?
- Pulse output frequency = about 500kpps
- Input: ABZ-phase pulse type encoder (At the moment, I have no plans to input an encoder such as EnDat, BiSS, HIPERFACE, Tamagawa, etc. directly into the MPU.)

Also, is processing faster when using the PRU than when using the A53 or R5F?
If it is faster, please let me know if there are any application notes or anything.

Best regards,
O.H