This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Help in CAN interface of the AM64x SK EVM board , with the AM6442B processor

Part Number: AM6442

Tool/software:

Our team recently bought a AM64x SK EVM launchpad board and on some initial research found there isn't a proper procedure given online in order to initialise the CAN interface on this board.
We have tried flashing the MCAN loopback codes present in CCS where they both with pass but our vector device connected to SOC_MAIN_UART5_TXD and SOC_MAIN_UART5_RXD did not detect any valid CAN packets, we also tried using a CAN transiever RX to RX and tx to tx connection , that also failed.

Please do help in this regard on how to get CAN running on this board.