Tool/software:
Hi experts,
We use SK-AM62A-LP board with a custom RGB+IR camera module.
The camera module use ub971 and am62a board use CSI2 to connect ub9702 to link camera.
They run in FPD-link IV mode.
When we run gst-launch-1.0 command to display, the stream show broken image and flickering.
I check the ub9702 register, it shows:
reg 0x4d = 0x33 or 0x13
reg 0x4e = 0xed
reg 0x7a = 0x0f
The LOCK_STS_CHG bit is always 1.
Dose it mean the link unstable?
Is there any way to improve it or tune it.
Regards,
Terry