Other Parts Discussed in Thread: OMAP-L138, SYSCONFIG
Hi TI Support,
We are trying to boot DSP code from the ARM. We have played with the LED sample on the TI wiki. We have code to compile the DSP code into a C byte array, and load it to the correct portion of SRAM (0x80010000). We then set the DSP start address in SYSCONFIG->HOST1CFG and then reset the DSP by setting LRST bit in PSC0->MDCTL[15] low and then high. The DSP LED app works properly when loaded from CCSv3, but when loaded by the ARM, it doesn’t seem to start. Could you provide more details on how exactly to tell the DSP to reset and start executing code at a particular address?
int main() {
uint32_t bootAddr =
dsp_init();
EVMOMAPL138_dspDisable();
EVMOMAPL138_dspBootAddr(bootAddr);
EVMOMAPL138_dspEnable();
while(1) {}
}
void EVMOMAPL138_dspBootAddr(uint32_t addr)
{
// unlock the system config registers.
SYSCONFIG->KICKR[0] = KICK0R_UNLOCK;
SYSCONFIG->KICKR[1] = KICK1R_UNLOCK;
// Set DSP boot address vector to entry
point of DSP program
// This must be aligned to 1KB
boundaries
SYSCONFIG->HOST1CFG = addr;
// unlock the system config
registers.
SYSCONFIG->KICKR[0] = KICK0R_LOCK;
SYSCONFIG->KICKR[1] = KICK1R_LOCK;
}
void EVMOMAPL138_dspEnable(void)
{
// power dsp clocks and release core
from local reset
EVMOMAPL138_lpscTransition(PSC0,
DOMAIN1, LPSC_DSP, PSC_ENABLE); // clk on
SETBIT(PSC0->MDCTL[LPSC_DSP],
LRST);
// release reset
}
void EVMOMAPL138_dspDisable(void)
{
// halt dsp core using local reset,
then shut down dsp clocks
CLRBIT(PSC0->MDCTL[LPSC_DSP],
LRST);
// hold reset
EVMOMAPL138_lpscTransition(PSC0,
DOMAIN1, LPSC_DSP, PSC_DISABLE); // clk off
}
Thanks,
Martin
P.S. Here is the DSP coff binary converted to a C struct for reference (OMAPL138-DSP-LED/DSP sample compiled into coff out with CCSv3, then dumped with hex6x, and finally reformatted into C struct with perl):
/** === WARNING: AUTO-GENERATED by hex2c.pl === DO NOT MODIFY ===
*================================================================
* libdsp_c6748.hex.c
*
* DSP binary converted into a C byte array structure.
* Generated from the following tools:
* cl6x - generated coff from c
* hex6x - generates ascii hex from coff
* hex2c - generates this c file from hex
*
*================================================================
*/
#include <stdint.h>
#include <string.h>
const uint32_t dsp_start_addr = 0x80010000;
// Load to 0x80010000
const uint8_t dsp_80010000 [] = {
0x2A,0x3E,0x84,0x07,0xEA,0x00,0xC0,0x07, // 0x80010000
0xA2,0x07,0xBF,0x07,0x2A,0x14,0x08,0x07, // 0x80010008
0xEA,0x00,0x40,0x07,0xFA,0x00,0x00,0x02, // 0x80010010
0xA2,0x03,0x10,0x09,0xA2,0x03,0x10,0x0A, // 0x80010018
0x2A,0x70,0x06,0x02,0xEA,0x00,0x40,0x02, // 0x80010020
0x62,0x03,0x10,0x00,0x2A,0x20,0x80,0x01, // 0x80010028
0x28,0xD0,0x07,0x02,0xEA,0x00,0xC0,0x01, // 0x80010030
0xE8,0x00,0x40,0x02,0x00,0x00,0x00,0x00, // 0x80010038
0x28,0x90,0x87,0x01,0xE8,0x00,0xC0,0x01, // 0x80010040
0x62,0x13,0x0C,0x00,0x2A,0x2C,0x80,0x01, // 0x80010048
0xEA,0x00,0xC0,0x01,0x00,0x40,0x00,0x00, // 0x80010050
0x2A,0x00,0x07,0x02,0xEA,0x00,0x40,0x02, // 0x80010058
0x62,0x03,0x10,0x00,0x2A,0x3A,0x80,0x01, // 0x80010060
0xEA,0x00,0xC0,0x01,0xA8,0x00,0x00,0x02, // 0x80010068
0x00,0x20,0x00,0x00,0x90,0x02,0x00,0x00, // 0x80010070
0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010078
};
// Load to 0x80010880
const uint8_t dsp_80010880 [] = {
0xF7,0x31,0x6E,0x2C,0xDB,0x00,0x5B,0x0B, // 0x80010880
0x20,0xA1,0x04,0x00,0x29,0x1C,0xA0,0x01, // 0x80010888
0xAA,0x89,0x05,0x02,0xE9,0xE0,0x80,0x01, // 0x80010890
0xEA,0xF3,0x41,0x02,0x00,0x80,0x60,0xE0, // 0x80010898
0x76,0x02,0x0C,0x02,0x6E,0x2C,0xC0,0x85, // 0x800108a0
0x28,0xF0,0xF8,0x01,0x68,0xD2,0xCA,0x01, // 0x800108a8
0x34,0x00,0x6E,0x2C,0x6E,0x01,0x00,0x02, // 0x800108b0
0x2A,0x00,0x91,0x02,0x08,0x00,0x40,0xE2, // 0x800108b8
0x00,0x40,0x00,0x00,0x52,0x98,0x00,0x02, // 0x800108c0
0x55,0x10,0x6E,0x2C,0x6C,0x00,0x80,0x01, // 0x800108c8
0x28,0x40,0x03,0x02,0x00,0x40,0x00,0x00, // 0x800108d0
0x74,0x22,0x0D,0x02,0x00,0x00,0x80,0xE0, // 0x800108d8
0x00,0x20,0x00,0x00,0x6C,0x00,0x80,0x01, // 0x800108e0
0x12,0x12,0x6E,0x4C,0x74,0x62,0x0C,0x02, // 0x800108e8
0x00,0x20,0x00,0x00,0x6C,0x00,0x80,0x01, // 0x800108f0
0x00,0x60,0x00,0x00,0x00,0x00,0x80,0xE0, // 0x800108f8
0x74,0x82,0x0C,0x02,0x00,0x20,0x00,0x00, // 0x80010900
0x6C,0x00,0x80,0x01,0x26,0x46,0x6E,0x4C, // 0x80010908
0x74,0x82,0x0D,0x02,0x00,0x20,0x00,0x00, // 0x80010910
0x6E,0x00,0x00,0x02,0x00,0x00,0x00,0xE1, // 0x80010918
0x6E,0x00,0x80,0x02,0x6E,0x4C,0x4D,0x38, // 0x80010920
0x6E,0x6C,0x43,0xA2,0x23,0xA2,0xC5,0x38, // 0x80010928
0x6E,0x2C,0xEF,0xA1,0xF7,0x31,0x6E,0x0C, // 0x80010930
0x32,0x22,0x27,0x46,0x00,0x20,0xC0,0xEF, // 0x80010938
0x5B,0x0B,0x72,0xFB,0x27,0x06,0x45,0xBC, // 0x80010940
0x6E,0x2C,0xA7,0x06,0xEA,0x02,0x80,0x02, // 0x80010948
0xFA,0x8A,0x14,0x00,0x20,0xA1,0x14,0x30, // 0x80010950
0x41,0x26,0x45,0xBC,0x01,0x80,0xE0,0xE8, // 0x80010958
0x6E,0x2C,0x89,0x8E,0x20,0xA1,0xFC,0x2F, // 0x80010960
0x32,0x22,0x5B,0x09,0x27,0xC6,0x72,0xFB, // 0x80010968
0x27,0x06,0x45,0xBC,0x6E,0x2C,0xA7,0x06, // 0x80010970
0xEA,0x02,0x80,0x02,0x60,0x80,0xA0,0xE7, // 0x80010978
0xFA,0x8A,0x14,0x00,0x20,0xA1,0x0A,0x30, // 0x80010980
0x41,0x26,0x45,0xBC,0x6E,0x2C,0x89,0x8E, // 0x80010988
0x20,0xA1,0x04,0x20,0x32,0x22,0x5B,0x07, // 0x80010990
0x27,0x46,0x32,0xFF,0x00,0x98,0x80,0xED, // 0x80010998
0x27,0x06,0x45,0xBC,0x6E,0x2C,0xA7,0x06, // 0x800109a0
0xEA,0x02,0x80,0x02,0xFA,0x8A,0x14,0x00, // 0x800109a8
0x20,0xA1,0x12,0x30,0x41,0x26,0x45,0xBC, // 0x800109b0
0x6E,0x2C,0x89,0x8E,0x00,0x00,0x60,0xEC, // 0x800109b8
0x20,0xA1,0xFA,0x2F,0x32,0x22,0x5B,0x03, // 0x800109c0
0x27,0xC6,0x32,0xFF,0x27,0x06,0x45,0xBC, // 0x800109c8
0x6E,0x2C,0xA7,0x06,0xEA,0x02,0x80,0x02, // 0x800109d0
0xFA,0x8A,0x14,0x00,0x18,0x80,0xC0,0xE3, // 0x800109d8
0x20,0xA1,0xAC,0x3F,0x41,0x26,0x45,0xBC, // 0x800109e0
0x6E,0x2C,0x89,0x8E,0x20,0xA1,0x02,0x20, // 0x800109e8
0x20,0xA1,0xAC,0x0F,0xF7,0x8C,0x65,0xEC, // 0x800109f0
0x45,0xDC,0x45,0xAC,0x00,0x00,0xC0,0xEC, // 0x800109f8
0x00,0x20,0x00,0x00,0x6C,0x00,0x80,0x01, // 0x80010a00
0x47,0x92,0x6E,0x4C,0x76,0xE2,0x0C,0x02, // 0x80010a08
0x00,0x20,0x00,0x00,0x6C,0x00,0x80,0x01, // 0x80010a10
0x26,0x46,0x6E,0x4C,0x00,0x00,0x80,0xE8, // 0x80010a18
0x74,0xA2,0x0C,0x02,0x00,0x20,0x00,0x00, // 0x80010a20
0x6C,0x00,0x80,0x01,0x4D,0xDC,0x6E,0x6C, // 0x80010a28
0x76,0x02,0x0D,0x02,0x00,0x20,0x00,0x00, // 0x80010a30
0x6C,0x00,0x80,0x01,0x00,0x00,0x00,0xE1, // 0x80010a38
0x00,0x60,0x00,0x00,0x64,0x22,0x0D,0x02, // 0x80010a40
0x88,0xAD,0x11,0x02,0x74,0x22,0x0D,0x02, // 0x80010a48
0x00,0x20,0x00,0x00,0x6E,0x00,0x00,0x02, // 0x80010a50
0xE6,0x42,0x10,0x02,0x00,0x00,0x10,0xE0, // 0x80010a58
0x0A,0x7F,0x13,0x02,0x5A,0x2A,0x10,0x00, // 0x80010a60
0x20,0xA1,0x12,0x20,0x6E,0x00,0x00,0x02, // 0x80010a68
0xE6,0x42,0x10,0x02,0x0A,0x7F,0x13,0x02, // 0x80010a70
0x5A,0x2A,0x10,0x00,0x00,0x00,0x10,0xE0, // 0x80010a78
0x20,0xA1,0xFB,0x3F,0xE6,0x62,0x3C,0x02, // 0x80010a80
0x6C,0x00,0x80,0x01,0x00,0x60,0x00,0x00, // 0x80010a88
0x76,0x02,0x0D,0x02,0x00,0x20,0x00,0x00, // 0x80010a90
0x6E,0x00,0x00,0x02,0x00,0x60,0x00,0x00, // 0x80010a98
0xE6,0x42,0x10,0x02,0x0A,0x7F,0x13,0x02, // 0x80010aa0
0x5A,0x2A,0x10,0x00,0x20,0xA1,0x14,0x20, // 0x80010aa8
0x6E,0x00,0x00,0x02,0xE6,0x42,0x10,0x02, // 0x80010ab0
0x0A,0x7F,0x13,0x02,0x00,0x00,0x10,0xE0, // 0x80010ab8
0x5A,0x2A,0x10,0x00,0x20,0xA1,0xFC,0x3F, // 0x80010ac0
0x58,0xA3,0x04,0x02,0x52,0x08,0x80,0x07, // 0x80010ac8
0x62,0xA3,0x8C,0x00,0x00,0x00,0x00,0x00, // 0x80010ad0
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010ad8
0x59,0x00,0x90,0x02,0x5B,0x6F,0x90,0x02, // 0x80010ae0
0xAB,0x0D,0x00,0x03,0xA1,0x01,0x18,0x01, // 0x80010ae8
0x42,0x09,0x90,0x03,0xA1,0x67,0x94,0x01, // 0x80010af0
0xF8,0xDB,0x18,0x03,0x79,0x7A,0x94,0x01, // 0x80010af8
0xDA,0x00,0x90,0x02,0xD8,0x2D,0x8C,0x01, // 0x80010b00
0xF8,0xCF,0x8C,0x00,0x10,0x22,0x00,0x80, // 0x80010b08
0x5A,0x6F,0x14,0x03,0x5A,0x10,0x90,0x02, // 0x80010b10
0x5A,0x2F,0x18,0x00,0x58,0x2F,0x88,0x01, // 0x80010b18
0x5A,0x10,0x0C,0x80,0x5B,0x20,0x10,0x22, // 0x80010b20
0xA3,0x47,0x98,0x00,0xA7,0x02,0x1C,0x24, // 0x80010b28
0xF8,0x50,0x18,0x01,0x87,0x36,0x90,0x43, // 0x80010b30
0xE3,0x03,0x04,0x03,0x5A,0x20,0x94,0x22, // 0x80010b38
0x5B,0xCF,0x9B,0x0F,0x58,0x10,0x10,0x02, // 0x80010b40
0xA2,0x59,0x08,0x02,0xA2,0x03,0xFC,0x00, // 0x80010b48
0x37,0x02,0x14,0x24,0x5A,0x40,0x13,0x00, // 0x80010b50
0xD6,0x36,0x94,0x43,0x64,0x36,0x90,0x01, // 0x80010b58
0x91,0x08,0x00,0x20,0x5B,0xE0,0x03,0x20, // 0x80010b60
0x64,0x36,0x90,0x01,0x91,0x08,0x00,0x20, // 0x80010b68
0x5B,0xE0,0x03,0x20,0x64,0x36,0x90,0x01, // 0x80010b70
0x91,0x08,0x00,0x20,0x5B,0xE0,0x03,0x20, // 0x80010b78
0x64,0x36,0x90,0x01,0x91,0x04,0x00,0x20, // 0x80010b80
0x5B,0xE0,0x03,0x20,0x64,0x36,0x90,0x01, // 0x80010b88
0x59,0x50,0x93,0x00,0x5B,0x10,0x0C,0x02, // 0x80010b90
0x91,0x04,0x00,0x20,0xA3,0xE1,0x03,0x20, // 0x80010b98
0x64,0x36,0x90,0x01,0x59,0xE0,0x87,0x80, // 0x80010ba0
0xF7,0x36,0x14,0x02,0x5B,0x10,0x0C,0x02, // 0x80010ba8
0x91,0x00,0x00,0x20,0xA3,0xE1,0x03,0x20, // 0x80010bb0
0x64,0x36,0x90,0x81,0x59,0x2F,0x88,0x00, // 0x80010bb8
0xF7,0x36,0x14,0x02,0x5A,0x10,0x0C,0x02, // 0x80010bc0
0xF7,0x36,0x14,0x02,0x5A,0x10,0x0C,0x02, // 0x80010bc8
0xF7,0x36,0x14,0x02,0x5A,0x10,0x0C,0x02, // 0x80010bd0
0xA3,0x03,0x98,0x00,0xF7,0x36,0x14,0x02, // 0x80010bd8
0x5A,0x10,0x0C,0x02,0x5B,0x5F,0x08,0x00, // 0x80010be0
0xF6,0x36,0x14,0x02,0x5A,0x10,0x10,0x02, // 0x80010be8
0x86,0x36,0x10,0x23,0xA7,0x02,0x10,0x82, // 0x80010bf0
0x10,0x1D,0x00,0x00,0x62,0x03,0x0C,0x00, // 0x80010bf8
0x58,0x00,0x14,0x02,0x00,0x00,0x00,0x00, // 0x80010c00
0xD6,0x36,0x14,0x23,0xB6,0x02,0x14,0x82, // 0x80010c08
0x59,0x4F,0x88,0x00,0xA6,0x36,0x90,0x23, // 0x80010c10
0xA6,0x36,0x10,0x83,0x5A,0x9F,0x08,0x01, // 0x80010c18
0x58,0x0F,0x0B,0x01,0xA6,0x36,0x90,0x84, // 0x80010c20
0xB6,0x36,0x94,0x23,0xB6,0x36,0x14,0x83, // 0x80010c28
0xA6,0x36,0x10,0x63,0xA6,0x36,0x10,0x64, // 0x80010c30
0xA6,0x36,0x90,0x63,0xA7,0x36,0x10,0x68, // 0x80010c38
0x90,0x0F,0x00,0xB0,0xB7,0x36,0x94,0x84, // 0x80010c40
0x58,0x10,0x10,0x02,0xB6,0x36,0x14,0x63, // 0x80010c48
0xB6,0x36,0x14,0x64,0xB6,0x36,0x94,0x63, // 0x80010c50
0xB6,0x36,0x14,0x68,0xE3,0x03,0x04,0x03, // 0x80010c58
0x24,0x36,0x90,0x01,0x5A,0xCF,0x1B,0x02, // 0x80010c60
0xA2,0x03,0x90,0x00,0x11,0x08,0x00,0x00, // 0x80010c68
0x24,0x36,0x90,0x01,0x11,0x08,0x00,0x00, // 0x80010c70
0x24,0x36,0x90,0x01,0x11,0x08,0x00,0x00, // 0x80010c78
0x24,0x36,0x90,0x01,0x5B,0x50,0x0B,0x00, // 0x80010c80
0x11,0x04,0x00,0x00,0x24,0x36,0x90,0x01, // 0x80010c88
0x59,0x40,0x8B,0x00,0x5B,0x10,0x0C,0x02, // 0x80010c90
0x11,0x04,0x00,0x00,0x24,0x36,0x90,0x01, // 0x80010c98
0x59,0xE0,0x87,0x80,0xB7,0x36,0x14,0x02, // 0x80010ca0
0x5B,0x10,0x0C,0x02,0x11,0x00,0x00,0x20, // 0x80010ca8
0xA3,0xE1,0x03,0x20,0x24,0x36,0x90,0x81, // 0x80010cb0
0xA2,0x03,0x98,0x00,0x62,0x03,0x0C,0x00, // 0x80010cb8
0x58,0x00,0x14,0x02,0x00,0x40,0x00,0x00, // 0x80010cc0
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010cc8
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010cd0
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010cd8
0x59,0xEA,0x93,0x00,0xF4,0x94,0xBC,0x05, // 0x80010ce0
0x59,0x00,0x04,0x01,0x91,0x16,0x00,0x80, // 0x80010ce8
0xF5,0x22,0x3C,0x05,0x40,0x09,0x10,0x05, // 0x80010cf0
0xA9,0xFF,0xFF,0xA1,0xF4,0x42,0x3C,0x06, // 0x80010cf8
0xE9,0xFF,0xFF,0xA1,0xF4,0x62,0xBC,0x06, // 0x80010d00
0x65,0x36,0xA8,0x90,0x58,0xEA,0x8F,0xA0, // 0x80010d08
0x58,0x10,0x8C,0x06,0x00,0x00,0x00,0x00, // 0x80010d10
0x28,0xFC,0x7F,0x06,0x00,0x00,0x00,0x00, // 0x80010d18
0x10,0x0D,0x00,0x90,0x58,0x00,0x84,0x01, // 0x80010d20
0x00,0x60,0x00,0x00,0x59,0x00,0x8C,0x05, // 0x80010d28
0x11,0xB8,0xFF,0x0F,0x64,0x02,0x28,0x02, // 0x80010d30
0x5A,0x90,0x28,0x02,0x2A,0xA6,0x86,0x01, // 0x80010d38
0x58,0x00,0x0C,0x03,0xEA,0x00,0xC0,0x01, // 0x80010d40
0x00,0x00,0x00,0x00,0x78,0x40,0xAD,0x01, // 0x80010d48
0x58,0x60,0x8D,0x01,0x78,0x8F,0x8D,0x01, // 0x80010d50
0x58,0x80,0x0C,0x05,0x64,0x20,0xA8,0x00, // 0x80010d58
0x00,0x60,0x00,0x00,0x2B,0xA6,0x86,0x81, // 0x80010d60
0x59,0x00,0x84,0x01,0x5B,0x90,0x28,0x82, // 0x80010d68
0x10,0xFD,0xFF,0x8F,0x10,0xB0,0xFF,0x8F, // 0x80010d70
0x64,0x02,0x28,0x82,0x58,0x00,0x8C,0x85, // 0x80010d78
0xEA,0x00,0xC0,0x81,0x58,0x00,0x0C,0x83, // 0x80010d80
0xA8,0xFF,0xFF,0x01,0xE8,0xFF,0xFF,0x01, // 0x80010d88
0x58,0xEA,0x8F,0x00,0x59,0x00,0x04,0x01, // 0x80010d90
0x91,0x0C,0x00,0x80,0x64,0x02,0x8C,0x90, // 0x80010d98
0x58,0x00,0x0C,0xB5,0xA8,0x00,0x80,0xA0, // 0x80010da0
0x00,0x20,0x00,0x00,0x90,0x08,0x00,0x90, // 0x80010da8
0x00,0x80,0x00,0x00,0x62,0x13,0x04,0x00, // 0x80010db0
0x2A,0xE4,0x86,0x01,0xEA,0x00,0xC0,0x01, // 0x80010db8
0x00,0x20,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010dc0
0x64,0x32,0xA8,0x00,0x00,0x60,0x00,0x00, // 0x80010dc8
0x90,0x00,0x00,0x80,0x62,0x13,0x04,0x80, // 0x80010dd0
0x2A,0xE4,0x86,0x81,0xEA,0x00,0xC0,0x81, // 0x80010dd8
0x00,0x20,0x00,0x00,0x5B,0x10,0xB4,0x01, // 0x80010de0
0xE4,0x22,0x3C,0x05,0x63,0x03,0x0C,0x00, // 0x80010de8
0xE4,0x23,0x3C,0x06,0xE4,0x92,0xBC,0x05, // 0x80010df0
0x00,0x60,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010df8
0x29,0x0E,0x88,0x01,0xF5,0x54,0xBC,0x05, // 0x80010e00
0xAA,0xFF,0x7F,0x02,0xE8,0x00,0xC0,0x01, // 0x80010e08
0x64,0x02,0x8C,0x01,0xF4,0x22,0x3C,0x05, // 0x80010e10
0xEA,0xFF,0x7F,0x02,0xAA,0xFF,0xFF,0x02, // 0x80010e18
0x7A,0x8A,0x94,0x02,0x58,0x0A,0x8C,0x01, // 0x80010e20
0xFA,0xBF,0x0C,0x00,0x29,0x10,0x88,0x21, // 0x80010e28
0x12,0x08,0x00,0x20,0x63,0x03,0x10,0x30, // 0x80010e30
0xE8,0x00,0xC0,0x21,0x64,0x02,0x8C,0x21, // 0x80010e38
0x58,0x00,0x10,0x05,0x2A,0x28,0x87,0x01, // 0x80010e40
0xEA,0x00,0xC0,0x01,0x00,0x00,0x00,0x00, // 0x80010e48
0x28,0x10,0x88,0x01,0xE8,0x00,0xC0,0x01, // 0x80010e50
0x64,0x02,0x8C,0x01,0x00,0x40,0x00,0x00, // 0x80010e58
0x2A,0x38,0x87,0x01,0x62,0x13,0x0C,0x00, // 0x80010e60
0xEA,0x00,0xC0,0x01,0x00,0x60,0x00,0x00, // 0x80010e68
0x2A,0x0C,0x08,0x02,0xEA,0x00,0x40,0x02, // 0x80010e70
0xE6,0x02,0x10,0x00,0x58,0x00,0x28,0x02, // 0x80010e78
0x2A,0x54,0x87,0x01,0xEA,0x00,0xC0,0x01, // 0x80010e80
0x00,0x00,0x00,0x00,0x29,0x0A,0x88,0x31, // 0x80010e88
0x12,0x07,0x00,0x30,0x63,0x03,0x00,0x20, // 0x80010e90
0xE8,0x00,0xC0,0x31,0x64,0x02,0x8C,0x30, // 0x80010e98
0x00,0x40,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010ea0
0x28,0x0A,0x88,0x01,0xE8,0x00,0xC0,0x01, // 0x80010ea8
0x64,0x02,0x8C,0x00,0x00,0x40,0x00,0x00, // 0x80010eb0
0x2A,0x68,0x87,0x01,0x10,0x06,0x00,0x90, // 0x80010eb8
0x62,0x13,0x04,0x80,0xEA,0x00,0xC0,0x01, // 0x80010ec0
0x00,0x40,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010ec8
0x28,0x12,0x88,0x01,0xE8,0x00,0xC0,0x01, // 0x80010ed0
0x64,0x02,0x8C,0x01,0x2A,0x78,0x87,0x01, // 0x80010ed8
0xEA,0x00,0xC0,0x01,0x00,0x20,0x00,0x00, // 0x80010ee0
0x62,0x13,0x0C,0x00,0x00,0x80,0x00,0x00, // 0x80010ee8
0x10,0x14,0x00,0x00,0x2A,0x80,0x87,0x01, // 0x80010ef0
0xEA,0x00,0xC0,0x01,0x00,0x40,0x00,0x00, // 0x80010ef8
0x10,0x00,0x00,0x00,0x00,0x80,0x00,0x00, // 0x80010f00
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f08
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f10
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f18
0xA8,0xFF,0xFF,0x02,0x2B,0x40,0x84,0x02, // 0x80010f20
0xA8,0xFF,0x7F,0x02,0xEB,0x00,0xC0,0x02, // 0x80010f28
0xE8,0xFF,0xFF,0x02,0x63,0x03,0x14,0x00, // 0x80010f30
0xA1,0x01,0x94,0x01,0x78,0xAA,0x90,0x00, // 0x80010f38
0xF9,0x00,0x00,0x02,0x64,0x02,0x0C,0x92, // 0x80010f40
0xF8,0x00,0x80,0x01,0x58,0x80,0x94,0x91, // 0x80010f48
0x5A,0x10,0x0C,0x02,0x00,0x00,0x00,0x00, // 0x80010f50
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f58
0x62,0x03,0x0C,0x00,0x00,0x80,0x00,0x00, // 0x80010f60
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f68
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f70
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f78
0x00,0x00,0x00,0x00,0x90,0x00,0x00,0x00, // 0x80010f80
0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f88
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f90
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010f98
0x04,0x00,0x00,0x00,0x14,0x10,0x01,0x80, // 0x80010fa0
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010fa8
0x04,0x00,0x00,0x00,0x18,0x10,0x01,0x80, // 0x80010fb0
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010fb8
0x04,0x00,0x00,0x00,0x1C,0x10,0x01,0x80, // 0x80010fc0
0x01,0x00,0x00,0x00,0x00,0x00,0x00,0x00, // 0x80010fc8
0x04,0x00,0x00,0x00,0x28,0x10,0x01,0x80, // 0x80010fd0
0x00,0x20,0xC2,0x01,0x00,0x00,0x00,0x00, // 0x80010fd8
0x04,0x00,0x00,0x00,0x2C,0x10,0x01,0x80, // 0x80010fe0
0x00,0x40,0xC1,0x01,0x00,0x00,0x00,0x00, // 0x80010fe8
0x04,0x00,0x00,0x00,0x20,0x10,0x01,0x80, // 0x80010ff0
0x60,0x0F,0x01,0x80,0x00,0x00,0x00,0x00, // 0x80010ff8
0x04,0x00,0x00,0x00,0x24,0x10,0x01,0x80, // 0x80011000
0x60,0x0F,0x01,0x80,0x00,0x00,0x00,0x00, // 0x80011008
0x00,0x00,0x00,0x00,
};
uint32_t dsp_init()
{
memcpy((void*)0x80010000, dsp_80010000, sizeof(dsp_80010000));
memcpy((void*)0x80010880, dsp_80010880, sizeof(dsp_80010880));
return dsp_start_addr;
}