This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: how to add a new device tree for max96712/9296a to A72 of tda4vl, then i2ctool can read/write them

Part Number: TDA4VL-Q1


Tool/software:

Hi Expert

sdk : processor-sdk-linux-j721s2/10_01_00_04

hardware : tda4lv + max96712/max9296a + max96701 + OX01F10

in linuk sdk, there is no device tree can be referred to create a new *.dtso file for max96712/max9296a, if want to let deserials can work with tda4, how to do

thank you 

Best Regard

Demon