This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J784S4: R5F PCIe support

Part Number: PROCESSOR-SDK-J784S4

Tool/software:

Hello everyone,

I just want to give you an update on the R5F PCIe interface configuration and device bring-up.

In the past I opened these two tickets related to the support and full functioning of the standard pci in R5F:
PROCESSOR-SDK-J784S4: PROCESSOR-SDK-J784S4: Implementing PCIE driver for the R5F - Inbound&Outbound - Processors forum - Processors - TI E2E support forums
PROCESSOR-SDK-J784S4: Implementing PCIE driver for the R5F - Processors forum - Processors - TI E2E support forums
To fully use the standard PCI features, it was necessary to implement the following SDK features:
- PCI bridge support on am64xx and j784s4 platforms
      * Map information of a device
      * Add endpoints devices
      * Configure Devices BARs
      * Configure root port space
      * Configure outbound address translation for accessing remote configuration space from RC

So we managed to the PCIe interface up and running on the R5F cores on the Jacinto and Sitara platforms we are using.
Consider this topic closed.
Many thanks to everyone who supported us on this. (, , )

Best regards, 
Joao Lima