Part Number: AM623
Other Parts Discussed in Thread: ADS131A04
Tool/software:
Hello,
I have 3 ADS131a04 devices connected on MCU_SPI0. They are setup according to section 10.1.3.1 of the datasheet where the first device is configured in Asynchronous Interrupt Mode and the other two devices in synchronous slave mode. I also have a program that I use to startup the M4F. The program uses RPMSG to start/stop M4 so I can load and test new code by stopping/starting the M4. My program issues multiple commands to the ADC as listed in the attached log. It starts by issuing UNLOCK followed by REST then NULLs until I get back FF04 from each device.
The first time I load my code it completes fine, and the register dump doesn't show any errors. However, if I stop/start M4 then my next run will fail to get FF04 from all 3 ADCs. I get FF04 from the first device but the second device reports 2220, which I believe is SPI fault. The 3rd device is probably not reachable. Now, if I stop/start M4 again, then this time I will get FF04 from devices 1 & 2, but device 3 now reports the SPI fault. On the 3rd stop/start of M4 then all 3 ADCs report FF04 and my code completes the other sequence of commands. My code doesn't do much other than making these calls when it starts:
Run-1 ===== cmd:0x0655 len:0x0c status: 0xff04ff042224 cmd:0x0011 len:0x0c status: 0x065506550655 cmd:0x0000 len:0x0c status: 0xff827f827f82 cmd:0x0000 len:0x0c status: 0xff04ff04ff04 cmd:0x0655 len:0x0c status: 0xff04ff04ff04 cmd:0x0000 len:0x0c status: 0x065506550655 cmd:0x4d02 len:0x0c status: 0x220022002200 cmd:0x0000 len:0x0c status: 0x2d022d022d02 cmd:0x4eae len:0x0c status: 0x220022002200 cmd:0x0000 len:0x0c status: 0x2eae2eae2eae cmd:0x4f0f len:0x0c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x2f0f2f0f2f0f cmd:0x0033 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x003300330033 cmd:0x0555 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x055505550555 cmd:0x0000 len:0x3c status: 0x220022002200 cmd:0x2500 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x250025002500 cmd:0x0000 len:0x3c status: 0x220022042204 ADC INIT COMPLETE ... Dumping registers cmd:0x2200 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x220022002200 [STAT_1 REG] cmd:0x2300 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x230023002300 [STAT_P REG] cmd:0x2400 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x240024002400 [STAT_N REG] cmd:0x2500 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x250025002500 [STAT_S REG] cmd:0x2f00 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x2f0f2f0f2f0f [ENABLE REG] echo stop > /sys/class/remote/remote0/state echo start > /sys/class/remote/remote0/state Run-2 ===== cmd:0x0655 len:0x0c status: 0x220000060009 cmd:0x0011 len:0x0c status: 0x065500060009 cmd:0x0000 len:0x0c status: 0xff8211000003 cmd:0x0000 len:0x0c status: 0xff0422200006 cmd:0x0000 len:0x0c status: 0xff0422200006 cmd:0x0000 len:0x0c status: 0xff0422200006 **** ADC NOT READY [ff0422200006] **** echo stop > /sys/class/remote/remote0/state echo start > /sys/class/remote/remote0/state Run-3 ===== cmd:0x0655 len:0x0c status: 0xff0422240006 cmd:0x0011 len:0x0c status: 0x065506550006 cmd:0x0000 len:0x0c status: 0xff827f821102 cmd:0x0000 len:0x0c status: 0xff04ff042220 cmd:0x0000 len:0x0c status: 0xff04ff042220 cmd:0x0000 len:0x0c status: 0xff04ff042220 **** ADC NOT READY [ff04ff042220] **** echo stop > /sys/class/remote/remote0/state echo start > /sys/class/remote/remote0/state Run-4 ===== cmd:0x0655 len:0x0c status: 0xff04ff042224 cmd:0x0011 len:0x0c status: 0x065506550655 cmd:0x0000 len:0x0c status: 0xff827f827f82 cmd:0x0000 len:0x0c status: 0xff04ff04ff04 cmd:0x0655 len:0x0c status: 0xff04ff04ff04 cmd:0x0000 len:0x0c status: 0x065506550655 cmd:0x4d02 len:0x0c status: 0x220022002200 cmd:0x0000 len:0x0c status: 0x2d022d022d02 cmd:0x4eae len:0x0c status: 0x220022002200 cmd:0x0000 len:0x0c status: 0x2eae2eae2eae cmd:0x4f0f len:0x0c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x2f0f2f0f2f0f cmd:0x0033 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x003300330033 cmd:0x0555 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x055505550555 cmd:0x0000 len:0x3c status: 0x220022002200 cmd:0x2500 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x250025002500 cmd:0x0000 len:0x3c status: 0x220022042204 ADS INIT COMPLETE ... Dumping registers cmd:0x2200 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x220022002200 [STAT_1 REG] cmd:0x2300 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x230023002300 [STAT_P REG] cmd:0x2400 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x240024002400 [STAT_N REG] cmd:0x2500 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x250025002500 [STAT_S REG] cmd:0x2f00 len:0x3c status: 0x220022002200 cmd:0x0000 len:0x3c status: 0x2f0f2f0f2f0f [ENABLE REG]