Tool/software:
I'm testing secure boot with SBL.
I could boot until U-Boot but the verifying hash of fitImage was failed.
U-Boot tried to find node named "signature" but it seems was failed.
name_fit_config=conf-ti_k3-am625-custom.dtb
## Loading kernel from FIT Image at 90000000 ...
Using 'conf-ti_k3-am625-custom.dtb' configuration
Verifying Hash Integrity ... fit_config_verify_required_keys: No signature node found: FDT_ERR_NOTFOUND
The node name is defined as FIT_SIG_NODENAME in include/image.h, and it is same with am62xx-evm.
What is the reason that the verifying is failed when devicetype is changed?
MCU+ SDK: v11.00.00.16
PSDK: v09.02.01.09
Best Regards,
Koji