Part Number: AM62A7
Tool/software:
Team,
I have read the below post:
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1299366/am62a7-spec-clarify-for-am62a-isp-performance
Original request is to use below sensor:
IMX902: 12.3Mpixel @40fps , 6k(H)x 2k(V) wide angle, which is not a standard image ratio.
but ISP has the limitation described in above post (315 MPixel/s, 4096 pixels/line).
1)Does any of our AM6xxx ISP would be able to support the above requirements?
For AM62A ISP (315 MPixel/s, 4096 pixels/line):
2) Are you aware of existing wide angle sensor (with 4096 pixels/line) that could be supported? for example 4kx2k?
I have seen IMX728 D3 camera is supported but 3840x2160 @30fps is not enough. Would need something closer to 4kx2k @38fps (ie as close as possible to theorical limit of the ISP).
3) I assume that AM67x ISP would enable to support 4kx2k@40fs (since it supports 480Mpixel/s)?
4)Are there some drivers/SW limitation or other system limitation that would prevent to use the ISP very close to the theroretical limit?
Thanks in advance,
Anber