Part Number: AUDIO-AM62D-EVM
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi experts,
I am using the following environment, but I am having trouble importing. Please help.
- FreeRTOS SDKv11.00.00
- CCSv20.1.1
- Sysconfig 23.0.1
- TI CLANG 4.1.0.LTS
When I tried to import sample code into CCS, the following error occurred. It is the same for A53 and C7x cores.
Problems importing project(s): Device 'Cortex R.AM62Dx' is not currently recognized
I am referring to the original thread.
- Check that it is added to the Preference -> Product
- Changing "id": "com.ti.MCU-PLUS-SDK-AM62DX", did not have any effect, so I am now returning it to the default.
- I have reinstalled the SDK and CCS once, and restarted my PC.
- I can create a .ccxml file and connect to the EVM.
- "default_sbl_null_hs_fs.cfg" has been executed.
Best regards,
O.H