Tool/software:
I was looking into using the code from the MCU+SDK for a secure boot implementation but I need to know if the code in the MCU+ SDK is DO-178C compliant. Does anyone if it is?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I was looking into using the code from the MCU+SDK for a secure boot implementation but I need to know if the code in the MCU+ SDK is DO-178C compliant. Does anyone if it is?
Addison,
I was looking into using the code from the MCU+SDK for a secure boot implementation
The secure boot implementation can be done using the TIFS SDK package and MCU PLUS SDK together.
You can get the TIFS SDK package from here: www.ti.com/.../AM263PX-RESTRICTED-SECURITY
Is the TIFS SDK Package DO178C Compliant? Also if I need to also use the MCU+ SDK then I need to know if it is also DO178C compliant
but I need to know if the code in the MCU+ SDK is DO-178C compliant. Does anyone if it is?
While TI does not specifically certifies the SDKs to DO-178C, we provide the safety enablers that can help you with your certification process. Please refer to below safety reports
AM263Px - Safety certification report - https://www.ti.com/lit/pdf/sffsaj6
Am263Px safety certificate https://www.ti.com/lit/pdf/sffsaj5
Safety Diagnostic Library certification reprot https://www.ti.com/lit/pdf/sffs714
Safety Offering overview - www.ti.com/.../sprt767
Is the TIFS SDK Package DO178C Compliant? Also if I need to also use the MCU+ SDK then I need to know if it is also DO178C compliant
We do not certify the SDKs to the DO178C.
Also for more details on how TI SDKs can be used for safety certification please refer to this thread: e2e.ti.com/.../mcu-plus-sdk-am263x-am263x