Part Number: TDA3XEVM
Tool/software:
I'm using a TDA3 custom board.
The sensor is currently connected to the cpi port.
The data is RAW14bit.
I set it up as follows, but an error occurs.
[IPU1-0] 2.296346 s: [IPU1-0] 2.296376 s: Entered chains_iss_Canlab_Display [IPU1-0] 2.297169 s: ISSCAPTURE: Create in progress !!! [IPU1-0] 2.347526 s: UTILS: DMA: Allocated CH (TCC) = 48 (48) [IPU1-0] 2.347648 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 48 (0x63304800) [IPU1-0] 2.347861 s: ISSCAPTURE: Create Done !!! [IPU1-0] 2.348319 s: DISPLAY: Create in progress !!! [IPU1-0] 2.348624 s: dispcore/src/vpscore_dss.c @ Line 1137: [IPU1-0] 2.348685 s: Un supported data format [IPU1-0] 2.348776 s: dispdrv/src/vpsdrv_displayCore.c @ Line 304: [IPU1-0] 2.348837 s: Set DSS parameter failed [IPU1-0] 2.348898 s: Assertion @ Line: 459 in displayLink_drv.c: status==SYSTEM_LINK_STATUS_SOK : failed !!! [IPU1-0] 2.349386 s: Assertion @ Line: 459 in displayLink_drv.c: status==SYSTEM_LINK_STATUS_SOK : failed !!!