Other Parts Discussed in Thread: , SK-AM62B-P1, SK-AM62-LP, SK-AM62B, SK-AM62-SIP
Tool/software:
Hello, I have recently build an Custom Am625 board with limited peripherals as needed. The issue is that I was not able to get the Power out at U7(TPS22918DBVR) which is basically a SD card power. I have done some changes by applying the pullups at VDD_3V3 to SD_CD and VDD_SD to SD_CMD,SD_D3,SD_D2,SD_D1,SD_D0,SD_CLK. Because of the voltage 3.3V is not at output at U7 I am not able to boot the device.
Below I am attaching the Schematic as reference.8463.Play.pdf
Please ignore the block diagram
Thanks and Regards
Mohit Sharma