This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Internal PD resistor value

Guru 10225 points

Part Number: AM3352

Tool/software:

Hi Support Team,

There is a problem with the AM3352BZCZA60 currently under development,
and a customer has requested confirmation of the following information. 
*When used at 3.3V

1. What are the min, typ, and max values of the internal PD resistor of RMII1_REF_CLK?

2. What are the min and max values of the built-in PD resistor of RMII1_REF_CLK at low temperature (-40°C) and at high temperature (+105°C)?

3. What is the maximum value of the current that can be drawn into RMII1_REF_CLK?


[ Background of question ]
I would like to select an external pull-up resistor that will make the voltage 2.475V or higher
in the ratio between the built-in pull-down resistor and the external pull-up resistor for this port.

Best Regards,
Kanae