This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J7200: Jacinto7 CPB - UART Communication Issues with GNSS Receiver

Part Number: PROCESSOR-SDK-J7200


Tool/software:

Dear TI Support Team,

I'm encountering UART communication problems on the Jacinto7 CPB and need assistance with proper configuration.

Hardware Setup:

  • Board: Jacinto7 CPB
  • Connected Device: GNSS receiver with antenna
  • Connection: TX, RX, and Ground pins
  • UART Interfaces: Attempted connections to UART1 and UART2 (which maps to UART3)

Issue Description: I have a GNSS receiver connected to the board via UART interface, but I'm not receiving any data output. The UART communication appears to be non-functional despite proper physical connections.

Connection Details:

  • GNSS TX → Board RX
  • GNSS RX → Board TX
  • GNSS GND → Board GND
  • Tested on both UART1 and UART2 interfaces

Troubleshooting Steps Taken:

  • Verified physical wiring connections
  • Tested on multiple UART interfaces (UART1, UART2)
  • Confirmed GNSS receiver functionality with other devices

Questions:

  1. What is the correct device tree configuration for enabling UART1, UAART2 and UART3 on the Jacinto7 CPB?
  2. Can you clarify the UART numbering scheme (you mentioned UART2 changes to UART3)?
  3. Are there specific pinmux settings required for UART functionality?
  4. How can I verify that the UART drivers are properly loaded and initialized?

Additional Information Needed:

  • Sample device tree configuration for UART interfaces
  • Any hardware jumper or switch settings required

The GNSS receiver typically outputs NMEA data at 115200 baud, so I need to ensure the UART is properly configured to receive this data stream.

Regards,
Sarthak