This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: [AM5728] MCSPI1 receives only 0x00 on MISO (SPI1_D1) despite valid waveform observed

Part Number: AM5728


Tool/software:

Hello,
I'm working with the AM5728 and facing an issue where MCSPI1 always reads 0x00 from the MISO pin (SPI1_D1), even though the slave device is sending data correctly.


PAD Configuration
CTRL_CORE_PAD_SPI1_D1 (F16) = 0x00040000
CTRL_CORE_PAD_SPI1_D0 (B25) = 0x00010000
CTRL_CORE_PAD_SPI1_CLK (A25) = 0x00010000
CTRL_CORE_PAD_SPI1_CS0 (A24) = 0x00010000


MCSPI Register Settings
MCSPI_MODULCTRL = 0x00000001
MCSPI_CHxCONF = 0x181E0FC0


Observations
The slave correctly receives data via MOSI.

An oscilloscope shows valid data on the MISO line.

However, when I read from MCSPI1 RX register, all values are 0x00.

Could you please help me understand what might be missing or misconfigured?

Thanks in advance.