This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A3: Boot Sequence and proceedure for custom board

Part Number: AM62A3


Tool/software:

Hi,

We are using the AM62A32AOMHIAMBR SoM on our custom board.

While working with the EVK kit, we were able to boot from the SD card by simply flashing the .wic image onto it, and the board booted successfully.

Now, on our custom board based on the same AM62A SoM, we have both eMMC and SD card boot options available. We would like to know:

Can we use the same approach of flashing the full .wic image to the SD card or eMMC and expect it to boot as it did on the EVK?
Or, do we need to manually load the Boot ROM binaries, SPL, and other bootloader components separately before the board can boot from SD or eMMC?

We are trying to understand the complete boot process for AM62A on a custom board and identify if there are any additional steps or differences we need to account for to achieve successful boot from SD card or eMMC.



Thanks,
Adnan