Tool/software: Linux
Hello experts,
i am newly started to work with texas board am62x-lp. i just bring-up the am62x-lp custom board. now i want to interface the tianma display that is connected to my board with 40 pin connector of LVDS. also one thing i notice that when i connect lcd with board or disconnect the board dmesg does not detect any changes. is there is a way to detect it like in hdmi hotplugin detection?
how to start interface it please guide me.
refer below attachment of tianma display
part number : YX-TFTRFQ-ZX-20230313001
display : 7’TFT with CTP TFT-LCD Module
YX-TFTRFQ-ZX-20230313001 pre-Spec V1.0 (1).pdf