This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Support for BCH16 ECC

Guru 10275 points

Part Number: AM3352

Tool/software:

Hi Support Team,

My customer is using MT29F4G08ABAFAH4-IT:F on a board with AM3352.
Here's the datasheet.
 m70a_4gb_3v_it_parallel_nand.pdf

Am I correct in thinking that in this case, this NAND is capable of up to 16-bit ECC correction
because of its large page size (4096 + 256 bytes)?

I understand that this is not a problem because there is a thread on the following site
that says that the ROM can be successfully activated when using BCH16 without any problem
with the equivalent product in a different package, and the TI representative has also posted
that this is the correct scheme.

AM3352: Boot issue with NAND ECC - Processors forum - Processors - TI E2E support forums

If the above understanding is correct, can we ignore the discrepancy
in the description of the TRM manufacturer code, which is also pointed out in the above thread?

Please let me check just to be sure.

Best Regards,
Kanae