This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
For DM36x based camera, we are planning to be ONVIF compliant by early Jan'21012. This will be based on ONVIF 1.02.
For PSIA, we are already PSIA compliant here.
Version 2.6 is the latest available, please use this now as it will be easier to migrate when new ONVIF is available
But for DM8127 based IP Camera, we will have ONVIF compliance done by June'2012 timeframe
Regards,
Raghu
hi Raghu:
"For DM36x based camera, we are planning to be ONVIF compliant by early Jan'21012. This will be based on ONVIF 1.02." ,
does the latest version DM36X support ONVIF? how can we get this version package?
Regards
Steven
Hi,
This release will be available early March, can you please check with Appro on Monday for this download
Regards,
Raghu
Hi Raghu:
We found the KTNF is evm version, we want to use this module, how can we get the release version? :)
Regards,
Steven
Hi,
KTNF production lib will be included in v3.0 releasing this week, please look for it on Monday at Appro site
regards,
Raghu
Hello,
Did you get the latest release 3.0? did it have the things you were looking for?
Please let us know if any issues.
Regards,
Raghu
Hi Raghu:
I will get this version next week, I want to automatic to disable the KT function at day, enable it at night by a switch to control it. how to get this function ?
Thanks
Regards
Steven
Hi,
From GUI ON/OFF for KTNF noise filter is supported, you can use this API.
Also, you can deleted the KTNF task when switcing to night mode, and reinserting again in day mode. But this change you need to modify in the code
Regards,
Raghu
Hi Raghu:
I use the v3.0 IPNC package, I install all the *.tgz, after "make sysall", I get the uImage_ipnc_dm365 under "/ipnc_rdk/tftp", But I when I use the image to boot as nfs, it hangs up.
On console, I type"tftp 0x80700000 uImage_ipnc_dm365", then type "bootm 0x80700000", below is boot info:
*******************************************************************************************************************************************
DM365 IPNC :>tftp 0x80700000 uImage_ipnc_dm365
TFTP from server 192.168.1.237; our IP address is 192.168.1.201
Filename 'uImage_ipnc_dm365'.
Load address: 0x80700000
Loading: #################################################################
#################################################################
#################################################################
##############
done
Bytes transferred = 3064828 (2ec3fc hex)
DM365 IPNC :>bootm 0x80700000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_IPNC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3064764 Bytes = 2.9 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
*******************************************************************************************************************************************
My board still uses V2.5 uboot, ubl. shall I need to use the V3.0 UBOOT and UBL ?
BestRegargs
Steven
Hi Raghu:
I intall the v3.0 Ref package according the "Users_Gudie_IPNC_DM36X.pdf" at page 38, after "cd ipnc_rdk", "make sysyall", then "cd ipnc_rdk/target/filesys/opt/ipnc", "#ls", there is no cmemk.ko, csl.ko, drv.ko, edmak.ko, irqk.ko. and I found under "dvsdk_ipnctools/"/kernel_binaries/dm365",
it is empty.
On the V2.5 Ref, after "make dvsdkall", the cmemk.ko, edmak.ko, irqk.ko will be intall at "/kernel_binaries/dm365", Under "ipnc_rdk/target/filesys/opt/ipnc", thereare files as below picture:
the dvsdk3.0 removes some files, I use "find -name av_capture_load.sh" under the INSTALL/ , nothing found. and can not found *.ko.
what is the reason?
Regards
Steven
Hi,
Can you please run "make sysall"
In this release, this sequence has changed to
make uboot
make lspcfg
make -C $(KERNELDIR) ARCH=arm CROSS_COMPILE=$(MVTOOL_PREFIX) prepare
make -C $(KERNELDIR) ARCH=arm CROSS_COMPILE=$(MVTOOL_PREFIX) modules_prepare
make dvsdkall
make all
make lspall
make
Regards,
Raghu
Also in your build config it gives this warning step
@echo
@echo "WARNING:"
@echo "Please run make lsp if you have changed cmem/edma/irqk/dm365mmap and use the new built uImage!!!!!"
You need to run "make lsp" for this to work
Regards,
Raghu
Hi Raghu:
The V3.0 Ref to boot fast, the flow changes so much, I just understand the flow, thanks very much.
Regards
Steven
"
Hi,
From GUI ON/OFF for KTNF noise filter is supported, you can use this API.
Also, you can deleted the KTNF task when switcing to night mode, and reinserting again in day mode. But this change you need to modify in the code
Regards,
Raghu"
The above two methods to enable or disable KTNF, do it need to reboot ipc every time ?