This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625-Q1: Regarding PLL worst case drift tolerance over a time period of 2 bis(1uS).

Part Number: AM625-Q1

Tool/software:

Hi Experts,

Our customer is going to use SMD (CRYSTAL / AV25080014 / 25.000000MHz / 20ppm / 300µW / SMD3.2x2.5x0.8) as CRYSTAL for AM625-Q1.

Our customer needs to know the PLL worst case drift tolerance over a time period of 2 bits (1uS). Coul you support and provide a table?

Best regards,

Ito

(085d294f-d0bc-41e5-98f3-17ed034d495f)

  • Hi Ito,

    Can you please point the document where the below is mentioned? I cannot find it the schematic checklist PDF

    Schematic Design and Review Checklist for AM62x

    https://www.ti.com/lit/an/sprado3/sprado3.pdf

    4)List CAN clock source tolerances (For crystals and resonators record manufacturing, temperature and aging tolerances. For PLL's, additionally record max drift over a 2 bit time period.  Tolerance must meet 2Mb CANFD clock requirement of +/-0.3% to be FD compatible even if the module is only used on an MSCAN network.

    Thanks,

    Stan

  • Hello Ito,

    Refer below the available measurement data:

    Could you please provide the clock tolerance specification for the MAIN_PLL0_HSDIV4_CLKOUT PLL that clocks the MCAN0 peripheral.
    We have reviewed the AM62x TRM and Clock Tree but haven't found this information.

    We determined the 6-sigma frequency error of the PLL output (80 MHz) that is sourcing the MCAN controller by measuring N-cycle jitter over a period of forty 80MHz clock cycles, which represents one bit time when operating at 2Mbps. The frequency error was calculated by applying the worst-case N-cycle jitter to the nominal period of forty clock cycles, or one bit time. The maximum frequency error of a single bit across the entire process, voltage, and temperature operating range (-40 to 125 junction) was 0.022%.

    We also measured the frequency error over a period that represents 10 bits at 2Mbps, which is the resynchronization period for MCAN. The maximum frequency error of the resynchronization period across the entire process, voltage, and temperature range (-40 to 125 junction) was 0.003%.

    Apologies for reopening this ticket. Could you please also verify the following? We need measurements for both 5 Mbps and 500 kbps data rates, as our project configuration is 5 Mbps FD CAN.
    I will need to check with the team that collected the data.

    We determined the 6-sigma frequency error of the PLL output (80 MHz) that is sourcing the MCAN controller by measuring N-cycle jitter over a period of ten 80MHz clock cycles, which represents one bit time when operating at 8Mbps. The frequency error was calculated by applying the worst-case N-cycle jitter to the nominal period of forty clock cycles, or one bit time. The maximum frequency error of a single bit across the entire process, voltage, and temperature operating range (-40 to 125 junction) was 0.064%.
    We also measured the frequency error over a period that represents 10 bits at 8Mbps, which is the resynchronization period for MCAN. The maximum frequency error of the resynchronization period across the entire process, voltage, and temperature range (-40 to 125 junction) was 0.010%.
    We did not measure jitter for the operating condition that represents 5Mbps, but the result would be somewhere between the 8Mbps and 2Mbps values.

    Note: We do not have any plans to measure jitter for any other operating conditions.  We did not collect data for a duration that represents two-bit periods because the error associated with a single bit represents the worst-case error for the peripheral.  The error associated to two bits would be between the single bit error and the 10-bit error.

    Regards,

    Sreenivasa