Tool/software:
Hi,
We have an Am437x gp evm board that has been in use for a long time, and the system is Ubi NAND. The startup also starts from NAND. Recently, I wanted to improve the system's read and write speed by successfully increasing the NAND bit width from 8 bits to 16 bits with the support of Hong. However, I found that the speed did not increase after booting from NAND, but instead became slower. I want to know if increasing the bit width cannot improve the startup speed? Is it due to the reason that the system speed has actually decreased? Uboot and Linux kernel, system, applications, etc. remain the same as before.
The general understanding is that increasing the data bit width should improve read and write speed.
the DTS timing for 8bit NAND:
nand@0,0 {
compatible = "ti,omap2-nand";
reg = <0 0 4>; /* device IO registers */
interrupt-parent = <&gpmc>;
interrupts = <0 IRQ_TYPE_NONE>, /* fifoevent */
<1 IRQ_TYPE_NONE>; /* termcount */
rb-gpios = <&gpmc 0 GPIO_ACTIVE_HIGH>; /* gpmc_wait0 */
ti,nand-xfer-type = "prefetch-dma";
ti,nand-ecc-opt = "bch16";
ti,elm-id = <&elm>;
nand-bus-width = <8>;
gpmc,device-width = <1>;
gpmc,sync-clk-ps = <0>;
/*CONFIG2*/
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <40>;
gpmc,cs-wr-off-ns = <40>;
/*CONFIG3*/
gpmc,adv-on-ns = <0>;
gpmc,adv-rd-off-ns = <25>;
gpmc,adv-wr-off-ns = <25>;
/*CONFIG4*/
gpmc,we-on-ns = <0>;
gpmc,we-off-ns = <20>;
gpmc,oe-on-ns = <3>;
gpmc,oe-off-ns = <30>;
/*CONFIG5*/
gpmc,access-ns = <30>;
gpmc,rd-cycle-ns = <40>;
gpmc,wr-cycle-ns = <40>;
/*CONFIG6*/
gpmc,bus-turnaround-ns = <0>;
gpmc,cycle2cycle-delay-ns = <0>;
gpmc,clk-activation-ns = <0>;
gpmc,wr-access-ns = <40>;
gpmc,wr-data-mux-bus-ns = <0>;
/* MTD partition table */
/* All SPL-* partitions are sized to minimal length
* which can be independently programmable. For
* NAND flash this is equal to size of erase-block */
#address-cells = <1>;
#size-cells = <1>;
the DTS timing for 16bit NAND:
nand@0,0 {
compatible = "ti,omap2-nand";
reg = <0 0 4>; /* device IO registers */
interrupt-parent = <&gpmc>;
interrupts = <0 IRQ_TYPE_NONE>, /* fifoevent */
<1 IRQ_TYPE_NONE>; /* termcount */
rb-gpios = <&gpmc 0 GPIO_ACTIVE_HIGH>; /* gpmc_wait0 */
ti,nand-xfer-type = "prefetch-dma";
ti,elm-id = <&elm>;
ti,nand-ecc-opt = "bch8";
nand-bus-width = <16>;
gpmc,wait-pin = <0>;
gpmc,sync-clk-ps = <0>;
gpmc,cs-on-ns = <0>;
gpmc,cs-rd-off-ns = <44>;
gpmc,cs-wr-off-ns = <44>;
gpmc,adv-on-ns = <6>;
gpmc,adv-rd-off-ns = <34>;
gpmc,adv-wr-off-ns = <44>;
gpmc,we-off-ns = <40>;
gpmc,oe-off-ns = <54>;
gpmc,access-ns = <64>;
gpmc,rd-cycle-ns = <82>;
gpmc,wr-cycle-ns = <82>;
gpmc,wr-access-ns = <40>;
gpmc,wr-data-mux-bus-ns = <0>;
Best Regard!
Dudechao