This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7-Q1: tiovxmosiac Error

Part Number: AM62A7-Q1


Tool/software:

When using tiovxmosaic via gstreamer, I get the following error.

On SK board, the command works fine.

We are using SDK version 10, and we are using a custom board, not an SK board.

What should I check?

gst:

gst-launch-1.0 \
v4l2src device=/dev/video4 io-mode=5 ! queue max-size-buffers=1 leaky=2 ! video/x-raw,width=1920,height=1080,framerate=30/1,format=UYVY ! \
tiovxdlcolorconvert ! \
video/x-raw,format=NV12, width=1920,height=1080 ! textoverlay text="VIDEO4 (/dev/video4)" ! queue ! mosaic.sink_0 \
v4l2src device=/dev/video3 io-mode=5  ! queue max-size-buffers=1 leaky=2 ! video/x-raw,width=1920,height=1080,framerate=30/1,format=UYVY ! \
tiovxdlcolorconvert ! \
video/x-raw,format=NV12, width=1920,height=1080 ! textoverlay text="VIDEO3 (/dev/video3)" ! queue ! mosaic.sink_1 \
tiovxmosaic name=mosaic \
sink_0::startx="<0>" sink_0::starty="<0>" sink_0::widths="<1920>" sink_0::heights="<540>" \
sink_1::startx="<0>" sink_1::starty="<540>" sink_1::widths="<1920>" sink_1::heights="<540>" ! \
queue ! video/x-raw, width=1920, height=1080 ! queue ! kmssink driver-name=tidss sync=false force-modesetting=true

APP: Init ... !!!
   969.185955 s: MEM: Init ... !!!
   969.186021 s: MEM: Initialized DMA HEAP (fd=8) !!!
   969.186171 s: MEM: Init ... Done !!!
   969.186186 s: IPC: Init ... !!!
   969.204608 s: IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
   969.209618 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
   969.209751 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_ERROR
   969.209770 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_WARNING
   969.209781 s:  VX_ZONE_INFO: Globally Enabled VX_ZONE_INFO
   969.210951 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-0 
   969.211281 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-1 
   969.211562 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-2 
   969.211804 s:  VX_ZONE_INFO: [tivxPlatformCreateTargetId:134] Added target MPU-3 
   969.211838 s:  VX_ZONE_INFO: [tivxInitLocal:126] Initialization Done !!!
   969.211852 s:  VX_ZONE_INFO: Globally Disabled VX_ZONE_INFO
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
[  957.770331] max96712 1-0029: max96712_get_vc_maps: VC map for port 0 is 0x04
[  957.777418] max96712 1-0029: Mapping sink 0/0 to output VC 0, type 2,30 
[  957.784134] max96712 1-0029: Mapping sink 0/1 to output VC 1, type 2,30 
[  957.790849] max96712 1-0029: max96712_get_vc_maps: VC map for port 0 is 0x04
[  957.797925] max96712 1-0029: Mapping sink 0/0 to output VC 0, type 2,30 
[  957.804637] max96712 1-0029: Mapping sink 0/1 to output VC 1, type 2,30 
[  957.811389] max96712 1-0029: enable streaming (0) 
[  957.816211] max96712 1-0029: Prepare for streaming
[  957.821012] max96712 1-0029: max96712_get_vc_maps: VC map for port 0 is 0x04
[  957.828069] max96712 1-0029: enable tx port 0
[  957.833446] max96712 1-0029: enable rx port 0
[  957.837822] max96712 1-0029: enable RX port 0 streams 0x3
[  957.843234] max9295E 1-0042: enable streaming 
   969.566105 s:  VX_ZONE_ERROR: [ownContextSendCmd:912] Command ack message returned failure cmd_status: -1
   969.566171 s:  VX_ZONE_ERROR: [ownNodeKernelInit:604] Target kernel, TIVX_CMD_NODE_CREATE failed for node img_mosaic_node
   969.566196 s:  VX_ZONE_ERROR: [ownNodeKernelInit:605] Please be sure the target callbacks have been registered for this core
   969.566208 s:  VX_ZONE_ERROR: [ownNodeKernelInit:606] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
   969.566225 s:  VX_ZONE_ERROR: [ownGraphNodeKernelInit:690] kernel init for node 0, kernel com.ti.img_proc.img.mosaic:2 ... failed !!!
   969.566252 s:  VX_ZONE_ERROR: [ graph_135 ] Node kernel init failed
   969.566264 s:  VX_ZONE_ERROR: [ graph_135 ] Graph verify failed
   969.566469 s:  VX_ZONE_ERROR: [ownReleaseReferenceInt:747] Invalid reference
ERROR: from element /GstPipeline:pipeline0/GstTIOVXMosaic:mosaic: Unable to init TIOVX module
Additional debug info:
/usr/src/debug/edgeai-gst-plugins/1.0.0/gst-libs/gst/tiovx/gs[  958.028382] max96712 1-0029: disable streaming (1) 
ttiovxmiso.c(1512): gst_tiovx_miso_negotiated_src_caps (): /GstP[  958.036344] max96712 1-0029: disable RX port 0 streams 0x3
ipeline:pipeline0/GstTIOVXMosaic:mosaic
Execution ended after 0[  958.047355] max9295E 1-0042: disable streaming 
:00:00.183445765
Setting pipeline to NULL ...
[  958.057425] max96712 1-0029: disable rx port 0
[  958.065998] max96712 1-0029: disable tx port 0
Freeing pipeline ...
   969.782587 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff882ea970 of type 00000816 at external count 1, internal count 0, releasing it
   969.782666 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=mosaic_node_config) now as a part of garbage collection
   969.782760 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff88321e50 of type 0000080f at external count 1, internal count 0, releasing it
   969.782774 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=mosaic_node_background_image_0) now as a part of garbage collection
   969.782795 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff8839cdd0 of type 00000813 at external count 1, internal count 0, releasing it
   969.782808 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=object_array_129) now as a part of garbage collection
   969.782829 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff88322120 of type 0000080f at external count 1, internal count 0, releasing it
   969.782842 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=image_130) now as a part of garbage collection
   969.783133 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff8839cf80 of type 00000813 at external count 1, internal count 0, releasing it
   969.783149 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=object_array_131) now as a part of garbage collection
   969.783169 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff883223f0 of type 0000080f at external count 1, internal count 0, releasing it
   969.783182 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=image_132) now as a part of garbage collection
   969.783480 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff883226c0 of type 0000080f at external count 1, internal count 0, releasing it
   969.783495 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=mosaic_node_output_image_0) now as a part of garbage collection
   969.783787 s:  VX_ZONE_WARNING: [vxReleaseContext:1275] Found a reference 0xffff882a95b0 of type 00000804 at external count 1, internal count 1, releasing it
   969.783802 s:  VX_ZONE_WARNING: [vxReleaseContext:1277] Releasing reference (name=com.ti.img_proc.img.mosaic:2) now as a part of garbage collection
   969.783816 s:  VX_ZONE_WARNING: [vxReleaseContext:1297] A kernel with name com.ti.img_proc.img.mosaic:2 has not been removed, possibly due to a kernel module not being unloaded.
   969.783828 s:  VX_ZONE_WARNING: [vxReleaseContext:1298] Removing as a part of garbage collection

  • Try using a tiovxmultiscaler to scale down each streams height to 540. You're going into the mosaic with the wrong height.

  • Hi Kim,

    What are the main differences between your board and the AM62A SK board? Are you using same size of DDR? 

      , tiovxmosaic can rescale the images if tiovxmultiscaler is not used.

    Regards,

    Jianzhong

  • Hi

    For DDR, we are using the same product as the SK board.

    MT53E1G32D2FW-046 AUT:B

    I removed a lot of parts from the SK board.

    Are there any points that you are suspicious of?

    Regards,

    Kim

  • Hi Kim,

    How about SW? What changes did you make from the SDK? The errors in your log indicate something is wrong with OpenVX.

    Regards,

    jianzhong

  • Hi

    We're currently testing with the default DTS mode to determine the cause of the issue.

    The fixes are the SD CARD GPIO and HDMI INT.

    The symptoms remain the same.

    // SPDX-License-Identifier: GPL-2.0-only OR MIT
    /*
     * AM62A SK: https://www.ti.com/lit/zip/sprr459
     *
     * Copyright (C) 2022-2024 Texas Instruments Incorporated - https://www.ti.com/
     */
    
    /dts-v1/;
    
    #include <dt-bindings/leds/common.h>
    #include <dt-bindings/gpio/gpio.h>
    #include <dt-bindings/net/ti-dp83867.h>
    #include "k3-am62a7.dtsi"
    
    / {
    	compatible = "ti,am62a7-sk", "ti,am62a7";
    	model = "Texas Instruments AM62A7 SK";
    
    	aliases {
    		serial0 = &wkup_uart0;
    		serial2 = &main_uart0;
    		serial3 = &main_uart1;
    		mmc0 = &sdhci0;
    		mmc1 = &sdhci1;
    		ethernet0 = &cpsw_port1;
    		spi0 = &ospi0;
    		rtc0 = &wkup_rtc0;
    		rtc1 = &tps659312;
    	};
    
    	chosen {
    		stdout-path = "serial2:115200n8";
    	};
    
    	memory@80000000 {
    		device_type = "memory";
    		/* 4G RAM */
    		reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
    		      <0x00000008 0x80000000 0x00000000 0x80000000>;
    	};
    
    	reserved-memory {
    		#address-cells = <2>;
    		#size-cells = <2>;
    		ranges;
    
    		/* global cma region */
    		linux,cma {
    			compatible = "shared-dma-pool";
    			reusable;
    			size = <0x00 0x24000000>;
    			alloc-ranges = <0x00 0xc0000000 0x00 0x24000000>;
    			linux,cma-default;
    		};
    
    		secure_tfa_ddr: tfa@9e780000 {
    			reg = <0x00 0x9e780000 0x00 0x80000>;
    			alignment = <0x1000>;
    			no-map;
    		};
    
    		secure_ddr: optee@9e800000 {
    			reg = <0x00 0x9e800000 0x00 0x01800000>; /* for OP-TEE */
    			alignment = <0x1000>;
    			no-map;
    		};
    
    		wkup_r5fss0_core0_dma_memory_region: r5f-dma-memory@9c800000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0x9c800000 0x00 0x100000>;
    			no-map;
    		};
    
    		wkup_r5fss0_core0_memory_region: r5f-dma-memory@9c900000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0x9c900000 0x00 0x01e00000>;
    			no-map;
    		};
    		mcu_r5fss0_core0_dma_memory_region: r5f-dma-memory@9b800000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0x9b800000 0x00 0x100000>;
    			no-map;
    		};
    
    		mcu_r5fss0_core0_memory_region: r5f-dma-memory@9b900000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0x9b900000 0x00 0x0f00000>;
    			no-map;
    		};
    
    		c7x_0_dma_memory_region: c7x-dma-memory@99800000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0x99800000 0x00 0x100000>;
    			no-map;
    		};
    
    		c7x_0_memory_region: c7x-memory@99900000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0x99900000 0x00 0x01f00000>;
    			no-map;
    		};
    
    		edgeai_rtos_ipc_memory_region: edgeai-rtos-ipc-memory-region {
    			reg = <0x00 0xa0000000 0x00 0x01000000>;
    			no-map;
    		};
    
    		edgeai_memory_region: edgeai-dma-memory@a1000000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0xa1000000 0x00 0x02000000>;
    			no-map;
    		};
    
    		edgeai_shared_region: edgeai_shared-memories {
    			compatible = "dma-heap-carveout";
    			reg = <0x00 0xa3000000 0x00 0x0b000000>;
    		};
    
    		edgeai_core_heaps: edgeai-core-heap-memory@ae000000 {
    			compatible = "shared-dma-pool";
    			reg = <0x00 0xae000000 0x00 0x12000000>;
    			no-map;
    		};
    	};
    
    	opp-table {
    		/* Add 1.4GHz OPP for am62p5-sk board. Requires VDD_CORE at 0v85 */
    		opp-1400000000 {
    			opp-hz = /bits/ 64 <1400000000>;
    			opp-supported-hw = <0x01 0x0004>;
    			clock-latency-ns = <6000000>;
    		};
    	};
    
    	vmain_pd: regulator-0 {
    		/* TPS25750 PD CONTROLLER OUTPUT */
    		compatible = "regulator-fixed";
    		regulator-name = "vmain_pd";
    		regulator-min-microvolt = <5000000>;
    		regulator-max-microvolt = <5000000>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vcc_5v0: regulator-1 {
    		/* Output of TPS63070 */
    		compatible = "regulator-fixed";
    		regulator-name = "vcc_5v0";
    		regulator-min-microvolt = <5000000>;
    		regulator-max-microvolt = <5000000>;
    		vin-supply = <&vmain_pd>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vcc_3v3_main: regulator-2 {
    		/* output of LM5141-Q1 */
    		compatible = "regulator-fixed";
    		regulator-name = "vcc_3v3_main";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		vin-supply = <&vmain_pd>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vdd_mmc1: regulator-3 {
    		/* TPS22918DBVR */
    		compatible = "regulator-fixed";
    		regulator-name = "vdd_mmc1";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		regulator-boot-on;
    		enable-active-high;
    		gpio = <&main_gpio0 31 GPIO_ACTIVE_HIGH>;
    	};
    
    	vcc_3v3_sys: regulator-4 {
    		/* output of TPS222965DSGT */
    		compatible = "regulator-fixed";
    		regulator-name = "vcc_3v3_sys";
    		regulator-min-microvolt = <3300000>;
    		regulator-max-microvolt = <3300000>;
    		vin-supply = <&vcc_3v3_main>;
    		regulator-always-on;
    		regulator-boot-on;
    	};
    
    	vddshv_sdio: regulator-5 {
    		compatible = "regulator-gpio";
    		regulator-name = "vddshv_sdio";
    		pinctrl-names = "default";
    		pinctrl-0 = <&vddshv_sdio_pins_default>;
    		regulator-min-microvolt = <1800000>;
    		regulator-max-microvolt = <3300000>;
    		regulator-boot-on;
    		vin-supply = <&ldo1>;
    		//gpios = <&main_gpio0 31 GPIO_ACTIVE_HIGH>;
    		states = <1800000 0x0>,
    			 <3300000 0x1>;
    	};
    
    	leds {
    		compatible = "gpio-leds";
    		pinctrl-names = "default";
    		pinctrl-0 = <&usr_led_pins_default>;
    
    		led-0 {
    			label = "am62a-sk:green:heartbeat";
    			gpios = <&main_gpio1 49 GPIO_ACTIVE_HIGH>;
    			linux,default-trigger = "heartbeat";
    			function = LED_FUNCTION_HEARTBEAT;
    			default-state = "off";
    		};
    	};
    
    	tlv320_mclk: clk-0 {
    		#clock-cells = <0>;
    		compatible = "fixed-clock";
    		clock-frequency = <12288000>;
    	};
    
    	hdmi0: connector-hdmi {
    		compatible = "hdmi-connector";
    		label = "hdmi";
    		type = "a";
    
    		port {
    			hdmi_connector_in: endpoint {
    				remote-endpoint = <&sii9022_out>;
    			};
    		};
    	};
    
    	codec_audio: sound {
    		compatible = "simple-audio-card";
    		simple-audio-card,name = "AM62Ax-SKEVM";
    		simple-audio-card,widgets =
    			"Headphone",	"Headphone Jack",
    			"Line",		"Line In",
    			"Microphone",	"Microphone Jack";
    		simple-audio-card,routing =
    			"Headphone Jack",	"HPLOUT",
    			"Headphone Jack",	"HPROUT",
    			"LINE1L",		"Line In",
    			"LINE1R",		"Line In",
    			"MIC3R",		"Microphone Jack",
    			"Microphone Jack",	"Mic Bias";
    		simple-audio-card,format = "dsp_b";
    		simple-audio-card,bitclock-master = <&sound_master>;
    		simple-audio-card,frame-master = <&sound_master>;
    		simple-audio-card,bitclock-inversion;
    
    		simple-audio-card,cpu {
    			sound-dai = <&mcasp1>;
    		};
    
    		sound_master: simple-audio-card,codec {
    			sound-dai = <&tlv320aic3106>;
    			clocks = <&tlv320_mclk>;
    		};
    	};
    };
    
    &mcu_pmx0 {
    	wkup_uart0_pins_default: wkup-uart0-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_MCU_IOPAD(0x0024, PIN_INPUT, 0) /* (C9) WKUP_UART0_RXD */
    			AM62AX_MCU_IOPAD(0x0028, PIN_OUTPUT, 0) /* (E9) WKUP_UART0_TXD */
    			AM62AX_MCU_IOPAD(0x002c, PIN_INPUT, 0) /* (C10) WKUP_UART0_CTSn */
    			AM62AX_MCU_IOPAD(0x0030, PIN_OUTPUT, 0) /* (C8) WKUP_UART0_RTSn */
    		>;
    	};
    };
    
    /* WKUP UART0 is used for DM firmware logs */
    &wkup_uart0 {
    	pinctrl-names = "default";
    	pinctrl-0 = <&wkup_uart0_pins_default>;
    	status = "reserved";
    };
    
    &main_pmx0 {
    	main_dss0_pins_default: main-dss0-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x100, PIN_OUTPUT, 0) /* (V17) VOUT0_VSYNC */
    			AM62AX_IOPAD(0x0f8, PIN_OUTPUT, 0) /* (T18) VOUT0_HSYNC */
    			AM62AX_IOPAD(0x104, PIN_OUTPUT, 0) /* (AA22) VOUT0_PCLK */
    			AM62AX_IOPAD(0x0fc, PIN_OUTPUT, 0) /* (U17) VOUT0_DE */
    			AM62AX_IOPAD(0x0b8, PIN_OUTPUT, 0) /* (U22) VOUT0_DATA0 */
    			AM62AX_IOPAD(0x0bc, PIN_OUTPUT, 0) /* (U21) VOUT0_DATA1 */
    			AM62AX_IOPAD(0x0c0, PIN_OUTPUT, 0) /* (U20) VOUT0_DATA2 */
    			AM62AX_IOPAD(0x0c4, PIN_OUTPUT, 0) /* (U19) VOUT0_DATA3 */
    			AM62AX_IOPAD(0x0c8, PIN_OUTPUT, 0) /* (T19) VOUT0_DATA4 */
    			AM62AX_IOPAD(0x0cc, PIN_OUTPUT, 0) /* (U18) VOUT0_DATA5 */
    			AM62AX_IOPAD(0x0d0, PIN_OUTPUT, 0) /* (V22) VOUT0_DATA6 */
    			AM62AX_IOPAD(0x0d4, PIN_OUTPUT, 0) /* (V21) VOUT0_DATA7 */
    			AM62AX_IOPAD(0x0d8, PIN_OUTPUT, 0) /* (V19) VOUT0_DATA8 */
    			AM62AX_IOPAD(0x0dc, PIN_OUTPUT, 0) /* (V18) VOUT0_DATA9 */
    			AM62AX_IOPAD(0x0e0, PIN_OUTPUT, 0) /* (W22) VOUT0_DATA10 */
    			AM62AX_IOPAD(0x0e4, PIN_OUTPUT, 0) /* (W21) VOUT0_DATA11 */
    			AM62AX_IOPAD(0x0e8, PIN_OUTPUT, 0) /* (W20) VOUT0_DATA12 */
    			AM62AX_IOPAD(0x0ec, PIN_OUTPUT, 0) /* (W19) VOUT0_DATA13 */
    			AM62AX_IOPAD(0x0f0, PIN_OUTPUT, 0) /* (Y21) VOUT0_DATA14 */
    			AM62AX_IOPAD(0x0f4, PIN_OUTPUT, 0) /* (Y22) VOUT0_DATA15 */
    			AM62AX_IOPAD(0x05c, PIN_OUTPUT, 1) /* (P22) GPMC0_AD8.VOUT0_DATA16 */
    			AM62AX_IOPAD(0x060, PIN_OUTPUT, 1) /* (R19) GPMC0_AD9.VOUT0_DATA17 */
    			AM62AX_IOPAD(0x064, PIN_OUTPUT, 1) /* (R20) GPMC0_AD10.VOUT0_DATA18 */
    			AM62AX_IOPAD(0x068, PIN_OUTPUT, 1) /* (R22) GPMC0_AD11.VOUT0_DATA19 */
    			AM62AX_IOPAD(0x06c, PIN_OUTPUT, 1) /* (T22) GPMC0_AD12.VOUT0_DATA20 */
    			AM62AX_IOPAD(0x070, PIN_OUTPUT, 1) /* (R21) GPMC0_AD13.VOUT0_DATA21 */
    			AM62AX_IOPAD(0x074, PIN_OUTPUT, 1) /* (T20) GPMC0_AD14.VOUT0_DATA22 */
    			AM62AX_IOPAD(0x078, PIN_OUTPUT, 1) /* (T21) GPMC0_AD15.VOUT0_DATA23 */
    		>;
    	};
    
    	main_uart0_pins_default: main-uart0-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x1c8, PIN_INPUT, 0) /* (E14) UART0_RXD */
    			AM62AX_IOPAD(0x1cc, PIN_OUTPUT, 0) /* (D15) UART0_TXD */
    		>;
    	};
    
    	main_uart1_pins_default: main-uart1-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x01e8, PIN_INPUT, 1) /* (C17) I2C1_SCL.UART1_RXD */
    			AM62AX_IOPAD(0x01ec, PIN_OUTPUT, 1) /* (E17) I2C1_SDA.UART1_TXD */
    			AM62AX_IOPAD(0x0194, PIN_INPUT, 2) /* (C19) MCASP0_AXR3.UART1_CTSn */
    			AM62AX_IOPAD(0x0198, PIN_OUTPUT, 2) /* (B19) MCASP0_AXR2.UART1_RTSn */
    		>;
    	};
    
    	main_i2c0_pins_default: main-i2c0-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x1e0, PIN_INPUT_PULLUP, 0) /* (B16) I2C0_SCL */
    			AM62AX_IOPAD(0x1e4, PIN_INPUT_PULLUP, 0) /* (A16) I2C0_SDA */
    		>;
    	};
    
    	main_i2c1_pins_default: main-i2c1-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x1e8, PIN_INPUT_PULLUP, 0) /* (B17) I2C1_SCL */
    			AM62AX_IOPAD(0x1ec, PIN_INPUT_PULLUP, 0) /* (A17) I2C1_SDA */
    		>;
    	};
    
    	main_i2c2_pins_default: main-i2c2-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x0b0, PIN_INPUT_PULLUP, 1) /* (K22) GPMC0_CSn2.I2C2_SCL */
    			AM62AX_IOPAD(0x0b4, PIN_INPUT_PULLUP, 1) /* (K24) GPMC0_CSn3.I2C2_SDA */
    		>;
    	};
    
    	main_mmc0_pins_default: main-mmc0-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x220, PIN_INPUT, 0) /* (Y3) MMC0_CMD */
    			AM62AX_IOPAD(0x218, PIN_INPUT, 0) /* (AB1) MMC0_CLKLB */
    			AM62AX_IOPAD(0x21c, PIN_INPUT, 0) /* (AB1) MMC0_CLK */
    			AM62AX_IOPAD(0x214, PIN_INPUT, 0) /* (AA2) MMC0_DAT0 */
    			AM62AX_IOPAD(0x210, PIN_INPUT_PULLUP, 0) /* (AA1) MMC0_DAT1 */
    			AM62AX_IOPAD(0x20c, PIN_INPUT_PULLUP, 0) /* (AA3) MMC0_DAT2 */
    			AM62AX_IOPAD(0x208, PIN_INPUT_PULLUP, 0) /* (Y4) MMC0_DAT3 */
    			AM62AX_IOPAD(0x204, PIN_INPUT_PULLUP, 0) /* (AB2) MMC0_DAT4 */
    			AM62AX_IOPAD(0x200, PIN_INPUT_PULLUP, 0) /* (AC1) MMC0_DAT5 */
    			AM62AX_IOPAD(0x1fc, PIN_INPUT_PULLUP, 0) /* (AD2) MMC0_DAT6 */
    			AM62AX_IOPAD(0x1f8, PIN_INPUT_PULLUP, 0) /* (AC2) MMC0_DAT7 */
    		>;
    	};
    
    	main_mmc1_pins_default: main-mmc1-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x23c, PIN_INPUT, 0) /* (A21) MMC1_CMD */
    			AM62AX_IOPAD(0x234, PIN_INPUT, 0) /* (B22) MMC1_CLK */
    			AM62AX_IOPAD(0x230, PIN_INPUT, 0) /* (A22) MMC1_DAT0 */
    			AM62AX_IOPAD(0x22c, PIN_INPUT, 0) /* (B21) MMC1_DAT1 */
    			AM62AX_IOPAD(0x228, PIN_INPUT, 0) /* (C21) MMC1_DAT2 */
    			AM62AX_IOPAD(0x224, PIN_INPUT, 0) /* (D22) MMC1_DAT3 */
    			AM62AX_IOPAD(0x240, PIN_INPUT, 0) /* (D17) MMC1_SDCD */
    		>;
    	};
    
    	usr_led_pins_default: usr-led-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x244, PIN_OUTPUT, 7) /* (D18) MMC1_SDWP.GPIO1_49 */
    		>;
    	};
    
    	main_usb1_pins_default: main-usb1-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x0258, PIN_OUTPUT, 0) /* (F18) USB1_DRVVBUS */
    		>;
    	};
    
    	main_mdio1_pins_default: main-mdio1-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x160, PIN_OUTPUT, 0) /* (V12) MDIO0_MDC */
    			AM62AX_IOPAD(0x15c, PIN_INPUT, 0) /* (V13) MDIO0_MDIO */
    		>;
    	};
    
    	main_rgmii1_pins_default: main-rgmii1-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x14c, PIN_INPUT, 0) /* (AB16) RGMII1_RD0 */
    			AM62AX_IOPAD(0x150, PIN_INPUT, 0) /* (V15) RGMII1_RD1 */
    			AM62AX_IOPAD(0x154, PIN_INPUT, 0) /* (W15) RGMII1_RD2 */
    			AM62AX_IOPAD(0x158, PIN_INPUT, 0) /* (V14) RGMII1_RD3 */
    			AM62AX_IOPAD(0x148, PIN_INPUT, 0) /* (AA16) RGMII1_RXC */
    			AM62AX_IOPAD(0x144, PIN_INPUT, 0) /* (AA15) RGMII1_RX_CTL */
    			AM62AX_IOPAD(0x134, PIN_INPUT, 0) /* (Y17) RGMII1_TD0 */
    			AM62AX_IOPAD(0x138, PIN_INPUT, 0) /* (V16) RGMII1_TD1 */
    			AM62AX_IOPAD(0x13c, PIN_INPUT, 0) /* (Y16) RGMII1_TD2 */
    			AM62AX_IOPAD(0x140, PIN_INPUT, 0) /* (AA17) RGMII1_TD3 */
    			AM62AX_IOPAD(0x130, PIN_INPUT, 0) /* (AB17) RGMII1_TXC */
    			AM62AX_IOPAD(0x12c, PIN_INPUT, 0) /* (W16) RGMII1_TX_CTL */
    		>;
    	};
    
    	main_mcasp1_pins_default: main-mcasp1-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x090, PIN_INPUT, 2) /* (L19) GPMC0_BE0n_CLE.MCASP1_ACLKX */
    			AM62AX_IOPAD(0x098, PIN_INPUT, 2) /* (R18) GPMC0_WAIT0.MCASP1_AFSX */
    			AM62AX_IOPAD(0x08c, PIN_OUTPUT, 2) /* (K19) GPMC0_WEn.MCASP1_AXR0 */
    			AM62AX_IOPAD(0x084, PIN_INPUT, 2) /* (L18) GPMC0_ADVn_ALE.MCASP1_AXR2 */
    		>;
    	};
    
    	main_gpio1_ioexp_intr_pins_default: main-gpio1-ioexp-intr-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x01d4, PIN_INPUT, 7) /* (C15) UART0_RTSn.GPIO1_23 */
    		>;
    	};
    
    	vddshv_sdio_pins_default: vddshv-sdio-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x07c, PIN_OUTPUT, 7) /* (M19) GPMC0_CLK.GPIO0_31 */
    		>;
    	};
    
    	ospi0_pins_default: ospi0-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_IOPAD(0x000, PIN_OUTPUT, 0) /* (H24) OSPI0_CLK */
    			AM62AX_IOPAD(0x02c, PIN_OUTPUT, 0) /* (F23) OSPI0_CSn0 */
    			AM62AX_IOPAD(0x00c, PIN_INPUT, 0) /* (E25) OSPI0_D0 */
    			AM62AX_IOPAD(0x010, PIN_INPUT, 0) /* (G24) OSPI0_D1 */
    			AM62AX_IOPAD(0x014, PIN_INPUT, 0) /* (F25) OSPI0_D2 */
    			AM62AX_IOPAD(0x018, PIN_INPUT, 0) /* (F24) OSPI0_D3 */
    			AM62AX_IOPAD(0x01c, PIN_INPUT, 0) /* (J23) OSPI0_D4 */
    			AM62AX_IOPAD(0x020, PIN_INPUT, 0) /* (J25) OSPI0_D5 */
    			AM62AX_IOPAD(0x024, PIN_INPUT, 0) /* (H25) OSPI0_D6 */
    			AM62AX_IOPAD(0x028, PIN_INPUT, 0) /* (J22) OSPI0_D7 */
    			AM62AX_IOPAD(0x008, PIN_INPUT, 0) /* (J24) OSPI0_DQS */
    		>;
    	};
    };
    
    &mcu_pmx0 {
    	status = "okay";
    
    	pmic_irq_pins_default: pmic-irq-default-pins {
    		pinctrl-single,pins = <
    			AM62AX_MCU_IOPAD(0x000, PIN_INPUT, 7) /* (E11) MCU_GPIO0_0 */
    		>;
    	};
    };
    
    &mcu_gpio0 {
    	status = "okay";
    };
    
    &main_i2c0 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_i2c0_pins_default>;
    	clock-frequency = <400000>;
    
    	typec_pd0: usb-power-controller@3f {
    		compatible = "ti,tps6598x";
    		reg = <0x3f>;
    
    		connector {
    			compatible = "usb-c-connector";
    			label = "USB-C";
    			self-powered;
    			data-role = "dual";
    			power-role = "sink";
    			port {
    				usb_con_hs: endpoint {
    					remote-endpoint = <&usb0_hs_ep>;
    				};
    			};
    		};
    	};
    
    	tps659312: pmic@48 {
    		compatible = "ti,tps6593-q1";
    		reg = <0x48>;
    		ti,primary-pmic;
    		system-power-controller;
    
    		gpio-controller;
    		#gpio-cells = <2>;
    
    		pinctrl-names = "default";
    		pinctrl-0 = <&pmic_irq_pins_default>;
    		interrupt-parent = <&mcu_gpio0>;
    		interrupts = <0 IRQ_TYPE_EDGE_FALLING>;
    
    		buck123-supply = <&vcc_3v3_sys>;
    		buck4-supply = <&vcc_3v3_sys>;
    		buck5-supply = <&vcc_3v3_sys>;
    		ldo1-supply = <&vcc_3v3_sys>;
    		ldo2-supply = <&vcc_3v3_sys>;
    		ldo3-supply = <&buck5>;
    		ldo4-supply = <&vcc_3v3_sys>;
    
    		regulators {
    			buck123: buck123 {
    				regulator-name = "vcc_core";
    				regulator-min-microvolt = <715000>;
    				regulator-max-microvolt = <895000>;
    				regulator-boot-on;
    				regulator-always-on;
    			};
    
    			buck4: buck4 {
    				regulator-name = "vcc_1v1";
    				regulator-min-microvolt = <1100000>;
    				regulator-max-microvolt = <1100000>;
    				regulator-boot-on;
    				regulator-always-on;
    			};
    
    			buck5: buck5 {
    				regulator-name = "vcc_1v8_sys";
    				regulator-min-microvolt = <1800000>;
    				regulator-max-microvolt = <1800000>;
    				regulator-boot-on;
    				regulator-always-on;
    			};
    
    			ldo1: ldo1 {
    				regulator-name = "vddshv5_sdio";
    				regulator-min-microvolt = <3300000>;
    				regulator-max-microvolt = <3300000>;
    				regulator-boot-on;
    				regulator-always-on;
    			};
    
    			ldo2: ldo2 {
    				regulator-name = "vpp_1v8";
    				regulator-min-microvolt = <1800000>;
    				regulator-max-microvolt = <1800000>;
    				regulator-boot-on;
    				regulator-always-on;
    			};
    
    			ldo3: ldo3 {
    				regulator-name = "vcc_0v85";
    				regulator-min-microvolt = <850000>;
    				regulator-max-microvolt = <850000>;
    				regulator-boot-on;
    				regulator-always-on;
    			};
    
    			ldo4: ldo4 {
    				regulator-name = "vdda_1v8";
    				regulator-min-microvolt = <1800000>;
    				regulator-max-microvolt = <1800000>;
    				regulator-boot-on;
    				regulator-always-on;
    			};
    		};
    	};
    };
    
    &main_i2c1 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_i2c1_pins_default>;
    	clock-frequency = <100000>;
    
    	exp1: gpio@22 {
    		compatible = "ti,tca6424";
    		reg = <0x22>;
    		gpio-controller;
    		#gpio-cells = <2>;
    		interrupt-parent = <&main_gpio1>;
    		interrupts = <23 IRQ_TYPE_EDGE_FALLING>;
    		interrupt-controller;
    		#interrupt-cells = <2>;
    		pinctrl-names = "default";
    		pinctrl-0 = <&main_gpio1_ioexp_intr_pins_default>;
    
    		gpio-line-names = "GPIO_CPSW2_RST", "GPIO_CPSW1_RST",
    				   "BT_EN_SOC", "MMC1_SD_EN",
    				   "VPP_EN", "EXP_PS_3V3_En",
    				   "EXP_PS_5V0_En", "EXP_HAT_DETECT",
    				   "GPIO_AUD_RSTn", "GPIO_eMMC_RSTn",
    				   "UART1_FET_BUF_EN", "BT_UART_WAKE_SOC",
    				   "GPIO_HDMI_RSTn", "CSI_GPIO0",
    				   "CSI_GPIO1", "WLAN_ALERTn",
    				   "HDMI_INTn", "TEST_GPIO2",
    				   "MCASP1_FET_EN", "MCASP1_BUF_BT_EN",
    				   "MCASP1_FET_SEL", "UART1_FET_SEL",
    				   "PD_I2C_IRQ", "IO_EXP_TEST_LED";
    	};
    
    	tlv320aic3106: audio-codec@1b {
    		#sound-dai-cells = <0>;
    		compatible = "ti,tlv320aic3106";
    		reg = <0x1b>;
    		ai3x-micbias-vg = <1>;	/* 2.0V */
    
    		/* Regulators */
    		AVDD-supply = <&vcc_3v3_sys>;
    		IOVDD-supply = <&vcc_3v3_sys>;
    		DRVDD-supply = <&vcc_3v3_sys>;
    		DVDD-supply = <&buck5>;
    	};
    
    	exp2: gpio@23 {
    		compatible = "ti,tca6424";
    		reg = <0x23>;
    		gpio-controller;
    		#gpio-cells = <2>;
    
    		gpio-line-names = "", "",
    				  "", "",
    				  "", "",
    				  "", "",
    				  "WL_LT_EN", "CSI_RSTz",
    				  "", "",
    				  "", "",
    				  "", "",
    				  "SPI0_FET_SEL", "SPI0_FET_OE",
    				  "RGMII2_BRD_CONN_DET", "CSI_SEL2",
    				  "CSI_EN", "AUTO_100M_1000M_CONFIG",
    				  "CSI_VLDO_SEL", "SoC_WLAN_SDIO_RST";
    	};
    
    	sii9022: bridge-hdmi@3b {
    		compatible = "sil,sii9022";
    		reg = <0x3b>;
    		//interrupt-parent = <&exp1>;
    		//interrupts = <16 IRQ_TYPE_EDGE_FALLING>;
    		#sound-dai-cells = <0>;
    		sil,i2s-data-lanes = < 0 >;
    
    		ports {
    			#address-cells = <1>;
    			#size-cells = <0>;
    
    			port@0 {
    				reg = <0>;
    
    				sii9022_in: endpoint {
    					remote-endpoint = <&dpi1_out>;
    				};
    			};
    
    			port@1 {
    				reg = <1>;
    
    				sii9022_out: endpoint {
    					remote-endpoint = <&hdmi_connector_in>;
    				};
    			};
    		};
    	};
    };
    
    &main_i2c2 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_i2c2_pins_default>;
    	clock-frequency = <400000>;
    };
    
    &sdhci0 {
    	/* eMMC */
    	status = "okay";
    	non-removable;
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_mmc0_pins_default>;
    	disable-wp;
    };
    
    &sdhci1 {
    	/* SD/MMC */
    	status = "okay";
    	vmmc-supply = <&vdd_mmc1>;
    	vqmmc-supply = <&vddshv_sdio>;
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_mmc1_pins_default>;
    	disable-wp;
    	no-1-8-v;
    };
    
    &main_gpio0 {
    	status = "okay";
    };
    
    &main_gpio1 {
    	status = "okay";
    };
    
    &main_gpio_intr {
    	status = "okay";
    };
    
    &main_uart0 {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_uart0_pins_default>;
    	interrupts-extended = <&gic500 GIC_SPI 178 IRQ_TYPE_LEVEL_HIGH>,
    			<&main_pmx0 0x1c8>; /* (D14) UART0_RXD PADCONFIG114 */
    	interrupt-names = "irq", "wakeup";
    };
    
    /* Main UART1 is used for TIFS firmware logs */
    &main_uart1 {
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_uart1_pins_default>;
    	status = "reserved";
    };
    
    /* Main Timer2 is used by C7x DSP */
    &main_timer2 {
    	status = "reserved";
    };
    
    &usbss0 {
    	status = "okay";
    	ti,vbus-divider;
    };
    
    &usb0 {
    	usb-role-switch;
    
    	port {
    		usb0_hs_ep: endpoint {
    			remote-endpoint = <&usb_con_hs>;
    		};
    	};
    };
    
    &usbss1 {
    	status = "okay";
    };
    
    &usb1 {
    	dr_mode = "host";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_usb1_pins_default>;
    };
    
    &cpsw3g {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_rgmii1_pins_default>;
    
    	cpts@3d000 {
    		/* MAP HW3_TS_PUSH to GENF1 */
    		ti,pps = <2 1>;
    	};
    };
    
    &cpsw_port1 {
    	status = "okay";
    	phy-mode = "rgmii-rxid";
    	phy-handle = <&cpsw3g_phy0>;
    };
    
    &cpsw_port2 {
    	status = "disabled";
    };
    
    &cpsw3g_mdio {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_mdio1_pins_default>;
    
    	cpsw3g_phy0: ethernet-phy@0 {
    		reg = <0>;
    		ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
    		ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
    		ti,min-output-impedance;
    	};
    };
    
    &mcasp1 {
    	status = "okay";
    	#sound-dai-cells = <0>;
    
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_mcasp1_pins_default>;
    
    	op-mode = <0>;          /* MCASP_IIS_MODE */
    	tdm-slots = <2>;
    
    	serial-dir = <  /* 0: INACTIVE, 1: TX, 2: RX */
    	       1 0 2 0
    	       0 0 0 0
    	       0 0 0 0
    	       0 0 0 0
    	>;
    	tx-num-evt = <0>;
    	rx-num-evt = <0>;
    };
    
    &dss {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&main_dss0_pins_default>;
    };
    
    &dss_ports {
    	/* VP2: DPI Output */
    	hdmi0_dss: port@1 {
    		reg = <1>;
    
    		dpi1_out: endpoint {
    			remote-endpoint = <&sii9022_in>;
    		};
    	};
    };
    
    &mailbox0_cluster0 {
    	ti,mbox-num-fifos = <2>;
    	mbox_r5_0: mbox-r5-0 {
    		ti,mbox-rx = <0 0 0>;
    		ti,mbox-tx = <1 0 0>;
    	};
    };
    
    &mailbox0_cluster1 {
    	ti,mbox-num-fifos = <2>;
    	mbox_c7x_0: mbox-c7x-0 {
    		ti,mbox-rx = <0 0 0>;
    		ti,mbox-tx = <1 0 0>;
    	};
    };
    
    &mailbox0_cluster2 {
    	ti,mbox-num-fifos = <2>;
    	mbox_mcu_r5_0: mbox-mcu-r5-0 {
    		ti,mbox-rx = <0 0 0>;
    		ti,mbox-tx = <1 0 0>;
    	};
    };
    
    &main_rti4 {
    	status = "reserved";
    };
    
    &c7x_0 {
    	mboxes = <&mailbox0_cluster1>, <&mbox_c7x_0>;
    	memory-region = <&c7x_0_dma_memory_region>,
    			<&c7x_0_memory_region>;
    };
    
    &wkup_r5fss0_core0 {
    	mboxes = <&mailbox0_cluster0>, <&mbox_r5_0>;
    	memory-region = <&wkup_r5fss0_core0_dma_memory_region>,
    		<&wkup_r5fss0_core0_memory_region>;
    };
    
    &mcu_r5fss0_core0 {
    	mboxes = <&mailbox0_cluster2>, <&mbox_mcu_r5_0>;
    	memory-region = <&mcu_r5fss0_core0_dma_memory_region>,
    			<&mcu_r5fss0_core0_memory_region>;
    };
    
    #define K3_TS_OFFSET(pa, val)	(0x4+(pa)*4) (0x10000 | val)
    
    &timesync_router {
    	status = "okay";
    	pinctrl-names = "default";
    	pinctrl-0 = <&cpsw_cpts>;
    
    	/* Use Time Sync Router to map GENF1 input to HW3_TS_PUSH output */
    	cpsw_cpts: cpsw-cpts {
    		pinctrl-single,pins = <
    			/* pps [cpsw cpts genf1] in17 -> out12 [cpsw cpts hw3_push] */
    			K3_TS_OFFSET(12, 17)
    			>;
    	};
    };
    
    &fss {
    	status = "okay";
    };
    
    &ospi0 {
    	pinctrl-names = "default";
    	pinctrl-0 = <&ospi0_pins_default>;
    
    	flash@0{
    		compatible = "spi-nand";
    		reg = <0x0>;
    		spi-tx-bus-width = <8>;
    		spi-rx-bus-width = <8>;
    		spi-max-frequency = <25000000>;
    		cdns,tshsl-ns = <60>;
    		cdns,tsd2d-ns = <60>;
    		cdns,tchsh-ns = <60>;
    		cdns,tslch-ns = <60>;
    		cdns,read-delay = <2>;
    
    		partitions {
    			compatible = "fixed-partitions";
    			#address-cells = <1>;
    			#size-cells = <1>;
    
    			partition@0 {
    				label = "ospi_nand.tiboot3";
    				reg = <0x0 0x80000>;
    			};
    
    			partition@80000 {
    				label = "ospi_nand.tispl";
    				reg = <0x80000 0x200000>;
    			};
    
    			partition@280000 {
    				label = "ospi_nand.u-boot";
    				reg = <0x280000 0x400000>;
    			};
    
    			partition@680000 {
    				label = "ospi_nand.env";
    				reg = <0x680000 0x40000>;
    			};
    
    			partition@6c0000 {
    				label = "ospi_nand.env.backup";
    				reg = <0x6c0000 0x40000>;
    			};
    
    			partition@2000000 {
    				label = "ospi_nand.rootfs";
    				reg = <0x2000000 0x5fc0000>;
    			};
    
    			partition@7fc0000 {
    				label = "ospi_nand.phypattern";
    				reg = <0x7fc0000 0x40000>;
    			};
    		};
    	};
    };
    

    If it's an OpenVX issue, should I suspect the DDR?

    Regards,

    Kim

  • It's possible. What's your DDR size? Did you change the memory map?

  • Sorry, I forgot that you are using the same DDR as the SK board

    For DDR, we are using the same product as the SK board.

    MT53E1G32D2FW-046 AUT:B

    So the question is, did you change the memory map?

  • Hi

    The above symptom occurs when booting using the boot command in uboot.

    This symptom also occurred with evkit.

    The reason for proceeding as described above is due to the hardware architecture.

    This issue does not occur during normal booting.