Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi TI expert,
I am working on am62a7-q1 custom board. I have tried to boot with SD card and UART.
When try to boot rom SD card: -
My board is stuck after below logs: -

Then i have tried to boot from the UART and flash the binary.
1. sbl_uart_uniflash_stage1.release.hs_fs.tiimage stage1 flashed completely
2. sbl_uart_uniflash_stage2.release.appimage.hs_fs not able to flash
below logs i am getting while flashing: -

I tried to debug the code and found that the DDR is not initialized proper.
I found that DDR0_RESET0_N (SOC ball - P6) goes high at particular point.
in the below image highlighted the line where DDR0_RESET0_N is goes high.

Our DDR part no is same as EVM board
There is only difference in the DDR temperature grade and revision no
Our board DDR part NO - MT53E1G32D2FW-046 AAT:C
EVM board DDR part no - MT53E1G32D2FW-046 AUT:B
I have tried with different DDR configuration generated by tool
some of the changes are below: -
--------------------------------------
FSP2 Frequency (MHz) 800Mhz
DDR Density (per channel) (Gb) 16
Operating Temperature Range -40c to 105C
not working
--------------------------------------------------
FSP2 Frequency (MHz) 800Mhz
DDR Density (per channel) (Gb) 16
Operating Temperature Range -40c to 105C
Termination: CA ODT (FSP2) - 40ohm
Not working
---------------------------------------------------
--------------------------------------------------
FSP2 Frequency (MHz) 800Mhz
DDR Density (per channel) (Gb) 16
Operating Temperature Range -40c to 105C
Termination: CA ODT (FSP2) - 80ohm
Not working
---------------------------------------------------
--------------------------------------------------
FSP2 Frequency (MHz) 800Mhz
DDR Density (per channel) (Gb) 16
Operating Temperature Range -40c to 105C
Termination: CA ODT (FSP2) - 40ohm
Termination: DQ ODT (FSP2) - 60Ohm
not working
---------------------------------------------------
I have built the SBL with these changes but still the same issue.
Could you please help us to generate the DDR configuration or is there any suggestion.
Regards
Satyajeet Singh