TMDS64EVM: EthernetIP Tunneling SBL Bootloader: Linux not pingable

Part Number: TMDS64EVM

Tool/software:

Hello Nick,

I have managed to boot the EthernetIP Adapter Tunneling Example with SBL from OSPI on the AM64x_EVM.

In order to get the example running on SBL I had to comment out the AppCtrl_sendIPNotify() in line 640 in app_task.c.

Now the example is running fine except that Linux cannot be pinged from host PC.

Linux dmesg log:

***************************************************************
***************************************************************

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project am64xx-evm ttyS2

Arago 2025.01 am64xx-evm ttyS2

am64xx-evm login: root
[   24.937248][   T29] kauditd_printk_skb: 2 callbacks suppressed
[   24.937270][   T29] audit: type=1006 audit(1748632024.375:14): pid=718 uid=0 subj=kernel old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[   24.957560][   T29] audit: type=1300 audit(1748632024.375:14): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffff6587528 a2=1 a3=1 items=0 ppid=1 pid=718 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
[   24.986046][   T29] audit: type=1327 audit(1748632024.375:14): proctitle="(systemd)"
[   25.069933][   T29] audit: type=1334 audit(1748632024.507:15): prog-id=18 op=LOAD
[   25.078905][   T29] audit: type=1300 audit(1748632024.507:15): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff9601ee8 a2=90 a3=0 items=0 ppid=1 pid=718 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[   25.107704][   T29] audit: type=1327 audit(1748632024.507:15): proctitle="(systemd)"
[   25.117244][   T29] audit: type=1334 audit(1748632024.507:16): prog-id=18 op=UNLOAD
[   25.125960][   T29] audit: type=1300 audit(1748632024.507:16): arch=c00000b7 syscall=57 success=yes exit=0 a0=8 a1=1 a2=0 a3=ffffaf403c60 items=0 ppid=1 pid=718 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[   25.154539][   T29] audit: type=1327 audit(1748632024.507:16): proctitle="(systemd)"
[   25.162903][   T29] audit: type=1334 audit(1748632024.507:17): prog-id=19 op=LOAD
root@am64xx-evm:~# dmesg
[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.12.35-ge3e551586dfa-dirty (kustural@DE1CL-269MGS3) (aarch64-oe-linux-gcc (GCC) 13.4.0, GNU ld (GNU Binutils) 2.42.0.20240723) #3 SMP PREEMPT Thu Aug  7 14:58:28 CEST 2025
[    0.000000] KASLR disabled due to lack of seed
[    0.000000] Machine model: Texas Instruments AM642 EVM
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: legacy bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a0000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 3 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a03fffff (3072 KiB) nomap non-reusable r5f-memory@a0100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0400000, size 12 MiB
[    0.000000] OF: reserved mem: initialized node virtual-eth-shm@a0400000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a0400000..0x00000000a0ffffff (12288 KiB) nomap non-reusable virtual-eth-shm@a0400000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a1000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable r5f-memory@a1100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a2000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a2ffffff (15360 KiB) nomap non-reusable r5f-memory@a2100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3000000..0x00000000a30fffff (1024 KiB) nomap non-reusable r5f-dma-memory@a3000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a3100000..0x00000000a3ffffff (15360 KiB) nomap non-reusable r5f-memory@a3100000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node m4f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a40fffff (1024 KiB) nomap non-reusable m4f-dma-memory@a4000000
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node m4f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0x00000000a4100000..0x00000000a4ffffff (15360 KiB) nomap non-reusable m4f-memory@a4100000
[    0.000000] OF: reserved mem: 0x00000000a5000000..0x00000000a57fffff (8192 KiB) nomap non-reusable ipc-memories@a5000000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a57fffff]
[    0.000000]   node   0: [mem 0x00000000a5800000-0x00000000ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000] cma: Reserved 32 MiB at 0x00000000fba00000 on node -1
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 22 pages/cpu s51672 r8192 d30248 u90112
[    0.000000] pcpu-alloc: s51672 r8192 d30248 u90112 alloc=22*4096
[    0.000000] pcpu-alloc: [0] 0 [0] 1
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=523086cd-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 524288
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: SWIOTLB bounce buffer size adjusted to 2MB
[    0.000000] software IO TLB: area num 2.
[    0.000000] software IO TLB: mapped [mem 0x00000000fb600000-0x00000000fb800000] (2MB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=512 to nr_cpu_ids=2.
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=2.
[    0.000000] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1 rcu_task_cpu_ids=2.
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: GICD_CTRL.DS=0, SCR_EL3.FIQ=1
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080040000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080050000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 225.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x33e45310bc, max_idle_ns: 440795207391 ns
[    0.000001] sched_clock: 58 bits at 225MHz, resolution 4ns, wraps every 4398046511101ns
[    0.009686] Console: colour dummy device 80x25
[    0.015033] Calibrating delay loop (skipped), value calculated using timer frequency.. 450.00 BogoMIPS (lpj=900000)
[    0.026435] pid_max: default: 32768 minimum: 301
[    0.032012] LSM: initializing lsm=capability,selinux
[    0.037886] SELinux:  Initializing.
[    0.042826] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.051130] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.063219] rcu: Hierarchical SRCU implementation.
[    0.068925] rcu:     Max phase no-delay instances is 1000.
[    0.075294] Timer migration: 1 hierarchy levels; 8 children per group; 1 crossnode level
[    0.085455] EFI services will not be available.
[    0.091316] smp: Bringing up secondary CPUs ...
[    0.105836] Detected VIPT I-cache on CPU1
[    0.105967] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
[    0.105990] GICv3: CPU1: using allocated LPI pending table @0x0000000080060000
[    0.106058] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.106314] smp: Brought up 1 node, 2 CPUs
[    0.139298] SMP: Total of 2 processors activated.
[    0.144829] CPU: All CPU(s) started at EL2
[    0.149758] CPU features: detected: 32-bit EL0 Support
[    0.155737] CPU features: detected: CRC32 instructions
[    0.161763] alternatives: applying system-wide alternatives
[    0.169087] Memory: 1875844K/2097152K available (13184K kernel code, 1444K rwdata, 5016K rodata, 3072K init, 642K bss, 180568K reserved, 32768K cma-reserved)
[    0.185791] devtmpfs: initialized
[    0.203354] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.214091] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.223091] 26880 pages in range for non-PLT usage
[    0.223125] 518400 pages in range for PLT usage
[    0.229265] pinctrl core: initialized pinctrl subsystem
[    0.241526] DMI not present or invalid.
[    0.249417] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.258331] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[    0.267492] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.277705] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.286673] audit: initializing netlink subsys (disabled)
[    0.293514] audit: type=2000 audit(0.208:1): state=initialized audit_enabled=0 res=1
[    0.294234] thermal_sys: Registered thermal governor 'step_wise'
[    0.302210] thermal_sys: Registered thermal governor 'power_allocator'
[    0.309159] cpuidle: using governor menu
[    0.321584] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.329360] ASID allocator initialised with 65536 entries
[    0.342939] /bus@f4000/interrupt-controller@1800000: Fixed dependency cycle(s) with /bus@f4000/interrupt-controller@1800000
[    0.368775] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.376489] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.383623] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.391278] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.398405] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.406060] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.413187] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.420845] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.431761] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR2.0 JTAGID[0x1bb3802f] Detected
[    0.442018] iommu: Default domain type: Translated
[    0.447708] iommu: DMA domain TLB invalidation policy: strict mode
[    0.455648] SCSI subsystem initialized
[    0.460654] libata version 3.00 loaded.
[    0.461026] usbcore: registered new interface driver usbfs
[    0.467398] usbcore: registered new interface driver hub
[    0.473630] usbcore: registered new device driver usb
[    0.480218] pps_core: LinuxPPS API ver. 1 registered
[    0.486023] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.496090] PTP clock support registered
[    0.500867] EDAC MC: Ver: 3.0.0
[    0.505427] scmi_core: SCMI protocol bus registered
[    0.511764] FPGA manager framework
[    0.516115] Advanced Linux Sound Architecture Driver Initialized.
[    0.524562] vgaarb: loaded
[    0.528706] clocksource: Switched to clocksource arch_sys_counter
[    0.536176] VFS: Disk quotas dquot_6.6.0
[    0.540978] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.560487] NET: Registered PF_INET protocol family
[    0.566579] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.577444] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    0.587059] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.595733] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.604724] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[    0.613543] TCP: Hash tables configured (established 16384 bind 16384)
[    0.621255] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.628924] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.637212] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.644539] RPC: Registered named UNIX socket transport module.
[    0.651395] RPC: Registered udp transport module.
[    0.656927] RPC: Registered tcp transport module.
[    0.662455] RPC: Registered tcp-with-tls transport module.
[    0.668784] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.676099] NET: Registered PF_XDP protocol family
[    0.681752] PCI: CLS 0 bytes, default 64
[    0.688363] Initialise system trusted keyrings
[    0.694114] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[    0.702009] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.709273] NFS: Registering the id_resolver key type
[    0.715237] Key type id_resolver registered
[    0.720241] Key type id_legacy registered
[    0.725097] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.732674] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.824007] Key type asymmetric registered
[    0.828959] Asymmetric key parser 'x509' registered
[    0.834791] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[    0.843403] io scheduler mq-deadline registered
[    0.848797] io scheduler kyber registered
[    0.853680] io scheduler bfq registered
[    0.862529] pinctrl-single 4084000.pinctrl: 33 pins, size 132
[    0.869997] pinctrl-single f4000.pinctrl: 180 pins, size 720
[    0.878909] ledtrig-cpu: registered to indicate activity on CPUs
[    0.895041] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.916458] loop: module loaded
[    0.922177] megasas: 07.727.03.00-rc1
[    0.933225] tun: Universal TUN/TAP device driver, 1.6
[    0.941090] VFIO - User Level meta-driver version: 0.3
[    0.949029] usbcore: registered new interface driver usb-storage
[    0.956896] i2c_dev: i2c /dev entries driver
[    0.963779] sdhci: Secure Digital Host Controller Interface driver
[    0.970932] sdhci: Copyright(c) Pierre Ossman
[    0.976492] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.984045] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.992898] usbcore: registered new interface driver usbhid
[    0.999365] usbhid: USB HID core driver
[    1.006258] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 (0,8000003f) counters available
[    1.017670] optee: probing for conduit method.
[    1.023000] optee: revision 4.6 (71785645fa6ce42d)
[    1.039933] optee: dynamic shared memory is enabled
[    1.052542] optee: initialized driver
[    1.052676] random: crng init done
[    1.060375] Initializing XFRM netlink socket
[    1.066526] NET: Registered PF_PACKET protocol family
[    1.072538] Key type dns_resolver registered
[    1.091321] registered taskstats version 1
[    1.096480] Loading compiled-in X.509 certificates
[    1.121928] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
[    1.259407] pca953x 0-0038: supply vcc not found, using dummy regulator
[    1.267170] pca953x 0-0038: using no AI
[    2.304759] pca953x 0-0038: failed writing register: -110
[    2.311306] pca953x 0-0038: probe with driver pca953x failed with error -110
[    2.319979] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
[    2.329485] pca953x 1-0022: supply vcc not found, using dummy regulator
[    2.337234] pca953x 1-0022: using AI
[    2.358393] omap_i2c 20010000.i2c: bus 1 rev0.12 at 400 kHz
[    2.366009] ti-sci-intr bus@f4000:interrupt-controller@a00000: Interrupt Router 3 domain created
[    2.376275] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
[    2.391140] ti-udma 485c0100.dma-controller: Number of rings: 68
[    2.400268] ti-udma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6)
[    2.411850] ti-udma 485c0000.dma-controller: Number of rings: 288
[    2.433020] ti-udma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15)
[    2.446106] printk: legacy console [ttyS2] disabled
[    2.452638] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 310, base_baud = 3000000) is a 8250
[    2.462302] printk: legacy console [ttyS2] enabled
[    2.473551] printk: legacy bootconsole [ns16550a0] disabled
[    2.490371] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000006
[    2.504964] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    2.548733] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    2.559654] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
[    2.568744] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
[    2.576593] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512, Policers 32
[    2.585953] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    2.619796] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
[    2.634583] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    2.646967] mmc0: CQHCI version 5.10
[    2.661660] j721e-pcie f102000.pcie: host bridge /bus@f4000/pcie@f102000 ranges:
[    2.669936] j721e-pcie f102000.pcie:       IO 0x0600001000..0x0600100fff -> 0x0000001000
[    2.678778] j721e-pcie f102000.pcie:      MEM 0x0600101000..0x06ffffffff -> 0x0000101000
[    2.687688] j721e-pcie f102000.pcie:   IB MEM 0x0000000000..0x0fffffffff -> 0x0000000000
[    2.708823] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    2.802104] mmc0: Command Queue Engine enabled
[    2.807390] mmc0: new HS200 MMC card at address 0001
[    2.814153] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[    2.822139] mmcblk0boot0: mmc0:0001 S0J56X 31.5 MiB
[    2.829652] mmcblk0boot1: mmc0:0001 S0J56X 31.5 MiB
[    2.837106] mmcblk0rpmb: mmc0:0001 S0J56X 4.00 MiB, chardev (239:0)
[    3.805562] j721e-pcie f102000.pcie: PCI host bridge to bus 0000:00
[    3.812645] pci_bus 0000:00: root bus resource [bus 00-ff]
[    3.818854] pci_bus 0000:00: root bus resource [io  0x0000-0xfffff] (bus address [0x1000-0x100fff])
[    3.828598] pci_bus 0000:00: root bus resource [mem 0x600101000-0x6ffffffff] (bus address [0x00101000-0xffffffff])
[    3.839681] pci 0000:00:00.0: [104c:b010] type 01 class 0x060400 PCIe Root Port
[    3.847706] pci 0000:00:00.0: BAR 0 [mem 0x00000000-0xfffffffff 64bit pref]
[    3.855371] pci 0000:00:00.0: PCI bridge to [bus 00]
[    3.861040] pci 0000:00:00.0:   bridge window [io  0x0000-0x0fff]
[    3.867835] pci 0000:00:00.0:   bridge window [mem 0x00000000-0x000fffff]
[    3.875327] pci 0000:00:00.0:   bridge window [mem 0x00000000-0x000fffff 64bit pref]
[    3.883857] pci 0000:00:00.0: supports D1
[    3.888570] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[    3.898540] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    3.907577] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[    3.914965] pci 0000:00:00.0: BAR 0 [mem size 0x1000000000 64bit pref]: can't assign; no space
[    3.924285] pci 0000:00:00.0: BAR 0 [mem size 0x1000000000 64bit pref]: failed to assign
[    3.933077] pci 0000:00:00.0: PCI bridge to [bus 01]
[    3.938786] pci_bus 0000:00: Some PCI device resources are unassigned, try booting with pci=realloc
[    3.948605] pci_bus 0000:00: resource 4 [io  0x0000-0xfffff]
[    3.954970] pci_bus 0000:00: resource 5 [mem 0x600101000-0x6ffffffff]
[    3.962327] pcieport 0000:00:00.0: of_irq_parse_pci: failed with rc=-22
[    3.970191] pcieport 0000:00:00.0: PME: Signaling with IRQ 511
[    3.977235] pcieport 0000:00:00.0: AER: enabled with IRQ 511
[    3.985407] clk: Disabling unused clocks
[    3.990613] mmc1: CQHCI version 5.10
[    4.012328] PM: genpd: Disabling unused power domains
[    4.018251] ALSA device list:
[    4.022033]   No soundcards found.
[    4.035437] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    4.044071] Waiting for root device PARTUUID=523086cd-02...
[    4.104630] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[    4.113061] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[    4.124039]  mmcblk1: p1 p2
[    5.197393] EXT4-fs (mmcblk1p2): recovery complete
[    5.204291] EXT4-fs (mmcblk1p2): mounted filesystem de0a189c-5c29-4371-8505-a156b6b7ec2d r/w with ordered data mode. Quota mode: none.
[    5.217226] VFS: Mounted root (ext4 filesystem) on device 179:98.
[    5.226958] devtmpfs: mounted
[    5.232898] Freeing unused kernel memory: 3072K
[    5.238355] Run /sbin/init as init process
[    5.243167]   with arguments:
[    5.243177]     /sbin/init
[    5.243185]   with environment:
[    5.243192]     HOME=/
[    5.243199]     TERM=linux
[    5.534818] systemd[1]: System time before build time, advancing clock.
[    5.598380] NET: Registered PF_INET6 protocol family
[    5.605904] Segment Routing with IPv6
[    5.610392] In-situ OAM (IOAM) with IPv6
[    5.663780] systemd[1]: systemd 255.21^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
[    5.696476] systemd[1]: Detected architecture arm64.
[    5.715877] systemd[1]: Hostname set to <am64xx-evm>.
[    6.345903] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    6.654773] systemd[1]: Queued start job for default target Graphical Interface.
[    6.703073] systemd[1]: Created slice Slice /system/getty.
[    6.724900] systemd[1]: Created slice Slice /system/modprobe.
[    6.749072] systemd[1]: Created slice Slice /system/serial-getty.
[    6.771892] systemd[1]: Created slice User and Session Slice.
[    6.789606] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[    6.809513] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[    6.829219] systemd[1]: Expecting device /dev/ttyS2...
[    6.845223] systemd[1]: Reached target Path Units.
[    6.861128] systemd[1]: Reached target Remote File Systems.
[    6.881112] systemd[1]: Reached target Slice Units.
[    6.897125] systemd[1]: Reached target Swaps.
[    6.958887] systemd[1]: Listening on RPCbind Server Activation Socket.
[    6.977238] systemd[1]: Reached target RPC Port Mapper.
[    7.010934] systemd[1]: Listening on Process Core Dump Socket.
[    7.029735] systemd[1]: Listening on initctl Compatibility Named Pipe.
[    7.051224] systemd[1]: Listening on Journal Audit Socket.
[    7.074225] systemd[1]: Listening on Journal Socket (/dev/log).
[    7.094348] systemd[1]: Listening on Journal Socket.
[    7.114543] systemd[1]: Listening on Network Service Netlink Socket.
[    7.141489] systemd[1]: Listening on udev Control Socket.
[    7.162094] systemd[1]: Listening on udev Kernel Socket.
[    7.182313] systemd[1]: Listening on User Database Manager Socket.
[    7.229452] systemd[1]: Mounting Huge Pages File System...
[    7.275036] systemd[1]: Mounting POSIX Message Queue File System...
[    7.299426] systemd[1]: Mounting Kernel Debug File System...
[    7.318363] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[    7.343165] systemd[1]: Mounting Temporary Directory /tmp...
[    7.390063] systemd[1]: Starting Create List of Static Device Nodes...
[    7.418433] systemd[1]: Starting Load Kernel Module configfs...
[    7.466142] systemd[1]: Starting Load Kernel Module drm...
[    7.482301] systemd[1]: Starting Load Kernel Module fuse...
[    7.531707] systemd[1]: Starting RPC Bind...
[    7.546117] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[    7.583221] systemd[1]: Starting Journal Service...
[    7.601105] fuse: init (API version 7.41)
[    7.638173] systemd[1]: Starting Load Kernel Modules...
[    7.670300] systemd[1]: Starting Generate network units from Kernel command line...
[    7.746250] systemd[1]: Starting Remount Root and Kernel File Systems...
[    7.793226] systemd[1]: Starting Coldplug All udev Devices...
[    7.847508] systemd[1]: Started RPC Bind.
[    7.858060] systemd-journald[110]: Collecting audit messages is enabled.
[    7.858592] systemd[1]: Mounted Huge Pages File System.
[    7.898708] systemd[1]: Mounted POSIX Message Queue File System.
[    7.926875] systemd[1]: Mounted Kernel Debug File System.
[    7.945091] EXT4-fs (mmcblk1p2): re-mounted de0a189c-5c29-4371-8505-a156b6b7ec2d.
[    7.961037] systemd[1]: Mounted Temporary Directory /tmp.
[    7.993367] systemd[1]: Finished Create List of Static Device Nodes.
[    8.016079] systemd[1]: modprobe@configfs.service: Deactivated successfully.
[    8.026402] systemd[1]: Finished Load Kernel Module configfs.
[    8.050452] systemd[1]: Started Journal Service.
[    8.437542] systemd-journald[110]: Received client request to flush runtime journal.
[    8.860891] audit: type=1334 audit(1748544505.319:2): prog-id=6 op=LOAD
[    8.876921] audit: type=1334 audit(1748544505.319:3): prog-id=7 op=LOAD
[    9.275628] audit: type=1334 audit(1748544505.735:4): prog-id=8 op=LOAD
[    9.332677] audit: type=1334 audit(1748544505.791:5): prog-id=9 op=LOAD
[    9.485034] audit: type=1334 audit(1748544505.947:6): prog-id=10 op=LOAD
[    9.499256] audit: type=1334 audit(1748544505.959:7): prog-id=11 op=LOAD
[    9.507730] audit: type=1334 audit(1748544505.959:8): prog-id=12 op=LOAD
[   10.683747] audit: type=1334 audit(1748632010.119:9): prog-id=13 op=LOAD
[   11.543251] audit: type=1334 audit(1748632010.979:10): prog-id=14 op=LOAD
[   11.556904] audit: type=1334 audit(1748632010.991:11): prog-id=15 op=LOAD
[   12.210700] Bluetooth: Core ver 2.22
[   12.218560] NET: Registered PF_BLUETOOTH protocol family
[   12.229034] Bluetooth: HCI device and connection manager initialized
[   12.241089] Bluetooth: HCI socket layer initialized
[   12.252115] Bluetooth: L2CAP socket layer initialized
[   12.262833] Bluetooth: SCO socket layer initialized
[   13.216848] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   13.267838] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[   13.282709] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[   13.581689] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[   13.629252] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[   15.140631] CAN device driver interface
[   15.305503] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[   15.489511] at24 0-0050: supply vcc not found, using dummy regulator
[   15.760834] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[   15.867866] platform 78000000.r5f: configured R5F for IPC-only mode
[   15.880516] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[   15.894216] remoteproc remoteproc0: 78000000.r5f is available
[   15.906430] remoteproc remoteproc0: attaching to 78000000.r5f
[   15.915974] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node r5f-dma-memory@a0000000
[   16.031164] virtio_rpmsg_bus virtio0: rpmsg host is online
[   16.032666] virtio_rpmsg_bus virtio0: creating channel ti.icve addr 0xd
[   16.045426] rpmsg_eth virtio0.ti.icve.-1.13: start_addr = 0xa0400000
[   16.052604] rpmsg_eth virtio0.ti.icve.-1.13: size 0xc00000
[   16.058288] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7)
[   16.068319] rpmsg_eth virtio0.ti.icve.-1.13: Default MAC Address = 00:00:00:00:00:00
[   16.069554] remoteproc remoteproc0: remote processor 78000000.r5f is now attached
[   16.076933] rpmsg_eth virtio0.ti.icve.-1.13: Assigning random MAC address
[   16.092733] rpmsg_eth virtio0.ti.icve.-1.13: New MAC Address = 36:aa:61:f5:e8:2f
[   16.406803] gpio-mux mux-controller: 2-way mux-controller registered
[   16.464253] m_can_platform 20701000.can: m_can device registered (irq=516, version=32)
[   16.490044] m_can_platform 20711000.can: m_can device registered (irq=517, version=32)
[   17.619168] m_can_platform 20701000.can main_mcan0: renamed from can0
[   17.690879] m_can_platform 20711000.can main_mcan1: renamed from can1
[   24.937248] kauditd_printk_skb: 2 callbacks suppressed
[   24.937270] audit: type=1006 audit(1748632024.375:14): pid=718 uid=0 subj=kernel old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[   24.957560] audit: type=1300 audit(1748632024.375:14): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffff6587528 a2=1 a3=1 items=0 ppid=1 pid=718 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
[   24.986046] audit: type=1327 audit(1748632024.375:14): proctitle="(systemd)"
[   25.069933] audit: type=1334 audit(1748632024.507:15): prog-id=18 op=LOAD
[   25.078905] audit: type=1300 audit(1748632024.507:15): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff9601ee8 a2=90 a3=0 items=0 ppid=1 pid=718 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[   25.107704] audit: type=1327 audit(1748632024.507:15): proctitle="(systemd)"
[   25.117244] audit: type=1334 audit(1748632024.507:16): prog-id=18 op=UNLOAD
[   25.125960] audit: type=1300 audit(1748632024.507:16): arch=c00000b7 syscall=57 success=yes exit=0 a0=8 a1=1 a2=0 a3=ffffaf403c60 items=0 ppid=1 pid=718 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[   25.154539] audit: type=1327 audit(1748632024.507:16): proctitle="(systemd)"
[   25.162903] audit: type=1334 audit(1748632024.507:17): prog-id=19 op=LOAD
root@am64xx-evm:~# ifconfig 192.168.1.20
192.168.1.20: error fetching interface information: Device not found
root@am64xx-evm:~# ifconfig eth1 192.168.1.20

FreeRTOS EthernetIP Tunneling Log:

Main Core init

Create Receive Task

Starting lwIP, local interface IP is dhcp-enabled
                                                 [LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[LWIPIF_LWIP_IC] Interface started successfully
Added interface 'br2', IP is 192.168.1.10

Before Wait for Linux

Before RPMsg Channel Announce

RPMsg Channel announced with Status
                                   [0]Network Link UP Event
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MAC to FDB
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MAC to FDB
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
     37.185s : CPU load =   1.91 %
     42.186s : CPU load =   4.29 %
     47.187s : CPU load =   4.30 %
     52.188s : CPU load =   4.29 %
     57.189s : CPU load =   4.28 %
     62.190s : CPU load =   4.28 %
     67.191s : CPU load =   4.27 %
     72.192s : CPU load =   4.30 %
     77.193s : CPU load =   4.30 %
     82.194s : CPU load =   4.30 %
     87.195s : CPU load =   4.30 %
     92.196s : CPU load =   4.29 %
     97.197s : CPU load =   4.28 %
    102.198s : CPU load =   4.28 %
    107.199s : CPU load =   4.28 %
    112.200s : CPU load =   4.29 %
    117.201s : CPU load =   4.29 %
    122.202s : CPU load =   4.28 %
    127.203s : CPU load =   4.28 %
    132.204s : CPU load =   4.30 %
    137.205s : CPU load =   4.30 %
    142.206s : CPU load =   4.30 %
    147.207s : CPU load =   4.31 %
    152.208s : CPU load =   4.31 %
    157.209s : CPU load =   4.29 %
    162.210s : CPU load =   4.29 %
    167.211s : CPU load =   4.28 %
    172.212s : CPU load =   4.28 %
Received Test Pkt
[IPC RPMSG ECHO] Remote Core ID    = 5
[IPC RPMSG ECHO] Remote Core EndPt = 1024
Adding new MCast entry to LwIP Bridge
MC addr added Successfully
Response message sent
    177.213s : CPU load =   4.33 %
    182.214s : CPU load =   4.30 %
    187.215s : CPU load =   4.30 %
    192.216s : CPU load =   4.29 %
    197.217s : CPU load =   4.29 %
    202.218s : CPU load =   4.29 %

Unsuccessful ping from host PC:

$ping 192.168.1.20
PING 192.168.1.20 (192.168.1.20) 56(84) bytes of data.
From 192.168.1.21 icmp_seq=1 Destination Host Unreachable
From 192.168.1.21 icmp_seq=2 Destination Host Unreachable
From 192.168.1.21 icmp_seq=3 Destination Host Unreachable
^C
--- 192.168.1.20 ping statistics ---
6 packets transmitted, 0 received, +3 errors, 100% packet loss, time 5151ms
pipe 4

Network interfaces in linux:

root@am64xx-evm:~# ip a
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
    inet 127.0.0.1/8 scope host lo
       valid_lft forever preferred_lft forever
    inet6 ::1/128 scope host noprefixroute
       valid_lft forever preferred_lft forever
2: eth0: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc mq state DOWN group default qlen 1000
    link/ether 1c:63:49:1a:d7:62 brd ff:ff:ff:ff:ff:ff
3: eth1: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc pfifo_fast state UP group default qlen 1000
    link/ether 1a:11:fe:66:ae:8b brd ff:ff:ff:ff:ff:ff
    inet 192.168.1.20/24 brd 192.168.1.255 scope global eth1
       valid_lft forever preferred_lft forever
    inet6 fe80::1811:feff:fe66:ae8b/64 scope link proto kernel_ll
       valid_lft forever preferred_lft forever
4: main_mcan0: <NOARP,ECHO> mtu 16 qdisc noop state DOWN group default qlen 10
    link/can
5: main_mcan1: <NOARP,ECHO> mtu 16 qdisc noop state DOWN group default qlen 10
    link/can

Another interesting behavior is the TX Buffer running full on linux:

[  615.259832][    C0] rpmsg_eth virtio0.ti.icve.-1.13 eth1: Tx buffer full 63
[  615.259845][    C0] rpmsg_eth virtio0.ti.icve.-1.13 eth1: Tx buffer full 63
[  615.259857][    C0] rpmsg_eth virtio0.ti.icve.-1.13 eth1: Tx buffer full 63
[  615.259868][    C0] rpmsg_eth virtio0.ti.icve.-1.13 eth1: Tx buffer full 63
[  615.259880][    C0] rpmsg_eth virtio0.ti.icve.-1.13 eth1: Tx buffer full 63
[  615.259891][    C0] rpmsg_eth virtio0.ti.icve.-1.13 eth1: Tx buffer full 63
[  615.259903][    C0] rpmsg_eth virtio0.ti.icve.-1.13 eth1: Tx buffer full 63

The same firmware is successfully running and pingable on the SPL bootflow!

My question are:

1. What could be wrong with the LwiP IC interface so that the RX Queue on FreeRTOS is running full?

2. How can I enable the debug of the LwiP stack, so to better understand the root cause of this behavior?

Thanks. 
BR

Luka

  • Hello again,
    The problem is still ongoing.
    Here some new infos:
    The cause is somewhere on the Linux side. The Ping is working fine in the Processor Linux SDK 9, but in SDK 11 is not pingable.
    Could you please investigate, where the problem could be here, that the Shared Memory Buffer is runnning full?


    What is also important to mention, that the change of IP in Linux is not received in FreeRTOS. So I assume that there is bug in the RPMsg driver?

  • Hi Luka,

    Apologies for the delayed response, this thread somehow missed my radar. 

    To confirm the observation along with the setup:

    1. When using the EthernetIP Tunneling Demo from Industrial Comms SDK 9.2, along with the Processor SDK Linux 9.2 - do the EIP Communication and Ping to Linux both work?

    2. When using the EthernetIP Tunneling Demo from Industrial Comms SDK 11.0, along with the Processor SDK Linux 11.00 - I understand that ping to Linux fails. Is the EIP communication working?

    In the meanwhile, I'll share your findings with the Linux side expert to get their input as well.

    Regards
    Archit

  • Hi Archit,

    here the answers to your questions:

    1. When using the EthernetIP Tunneling Demo from Industrial Comms SDK 9.2, along with the Processor SDK Linux 9.2 - do the EIP Communication and Ping to Linux both work?

    Both works. The ping from a host PC works as well as the EIP Communication (Link UP and DOWN is detected).

    2. When using the EthernetIP Tunneling Demo from Industrial Comms SDK 11.0, along with the Processor SDK Linux 11.00 - I understand that ping to Linux fails. Is the EIP communication working?

    The EIP communication is working fine.

    In the meantime, have you found something new?

    Regards
    Luka

  • Hi Luka,

    I discussed this with our Networking and Linux experts and here are some debug pointers from their side.

    This looks to be an issue with dequeueing packets from shared memory by R5 core. I suggest to do the following checks to identify where the system is failing.
    1. Are ping requests(or any other packets to linux) from external host received by Bridge netif in R5 application?

      If yes, then the pipeline from network to bridge is configured fairly correctly. Else, this indicates issues with setting up the lwip network stack and callbacks.

    2. Are ping requests from external host received by Linux?

      If yes, then Rx path to linux is good. Else, it indicates there is a break in shared memory pipeline.

    3. Is R5 core completing the function call “LWIPIF_LWIP_IC_recv” successfully?

      If yes, then the Tx from linux via shared memory is good. If not, then there is an issue with the shared memory driver configuration or setup.

    4. Is linux able to send any packets onto the wire?

      If yes, then the Tx buffer full is likely due to burst loads onto the shared memory. Else, it indicates the R5 core is not freeing the buffers in shared
      memory.

    If answer to (1) is “No”, then this needs a careful review of the LwIP setup and NRT pipeline handling for LwIP-EIP interface.

    If the answer to (2,3,4) of the questions is “No”, then the initialization of shared memory driver has to be check and made sure the driver is brought up correctly on R5. If the issue is only with one side, then probably the issue is with either some shared memory configuration mismatch, or issues with bridge netif.

    Let us know if any further clarification is required in above tests, and share the results once available.

    Regards
    Archit