Part Number: AM62P
Tool/software:
on our processor board, we are using DSI to connect a display.
We do not use the OLDI_ and VOUT0_ Interfaces. Can we simple leave the balls unconnected/the pins open?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62P
Tool/software:
on our processor board, we are using DSI to connect a display.
We do not use the OLDI_ and VOUT0_ Interfaces. Can we simple leave the balls unconnected/the pins open?
Hi Michael,
As per the datasheet, if OLDI0 is not used, balls are to be left unconnected. Since all VOUT0 pins are of non-open drain output type, DPI balls can also be left unconnected.
Best regards,
Luis Parga
Hi Michael,
For the OLDI0 signal, please refer to the Pin connectivity section of the data sheet:

e2e.ti.com/.../am623-vdda_1p8_oldi0-when-oldi0-is-unused
At a minimum can the requirement for filtering the power supply be removed so that the pin can be tied directly to an existing supply?
Don't see this as a concern. It is recommended to place a 0.1 uF decap near to the OLDI supply pin.
Regards,
Sreenivasa
Hi Michael,
The VOUT0 signals are LVCMOS buffer type.


You could leave them unconnected (no trace connected to pad)
In case traces are connected to the processor pads, an external pull is recommended.
Regards,
Sreenivasa