Other Parts Discussed in Thread: SK-AM62
Tool/software:
MCU SDK version: mcu_plus_sdk_am62x_10_01_00_33
Test EVM: SK-AM62
CCS version: 12.8.1
I imported the example from C:\ti\mcu_plus_sdk_am62x_10_01_00_33\examples\sdl\ecc\am62x-sk\r5fss0-0_freertos
Then, I compiled the R5 projects.
I use the file below to flash the default examples, then repower the EVM.
Use the CCS to load the ecc_app_am62x-sk_r5fss0-0_freertos_ti-arm-clang.out, and the CCS does not stop at the main function.
It just runs and there is no uart log from DM core.