Part Number: AM6442
Tool/software:
We have a custom board. On this we have a FPGA receiving a hardware signal from a connector.
This signal we can route through the FPGA to AM6442 pin P19 = GPMC0_CSn2, TIMER_IO8 or pin or R21 = GPMC0_CSn3, TIMER_IO9.
We want to timestamp the edge with the PTP counter.
We already use this devicetree entry to generate a PPS:
×ync_router {
pinctrl-names = "default";
pinctrl-0 = <&mcu_cpts_pps>;
mcu_cpts_pps: mcu-cpts-pps {
pinctrl-single,pins = <
TS_OFFSET(37, 22) /* pps [cpts genf1] in22 -> out37 [cpts hw8_push] */
TS_OFFSET(25, 22) /* pps [cpts genf1] in22 -> out25 [SYNC1_OUT pin] */
>;
};
};
Is it possible to do what we want, if so how to configure the path from GPIO to HW_PUSH?
Thanks and regards!