Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
I have a custom board and is trying to get the OTP Keywriter v10.00.08 (mcu_plus_sdk_am64x_10_00_00_20) to work through Ethernet/BOOTP.
The tiboot3.bin binary seems to be correctly uploaded to the device but there is no output on the serial console (Application does not appear to start at all).
According to the user guide, the keywriter application has been validated to work using UART,OSPI,USB-DFU,JTAG.
Ethernet/BOOTP is not included in the validated list but using OTP Keywriter v09_00_00 (mcu_plus_sdk_am64x_09_00_00_31) I can successfully run the keywriter application over Ethernet/BOOTP.
We would prefer to use version 10 as it allows for larger certificates.
Is there any reason why, running over Ethernet/BOOTP, should not work in version v10.00.08 but work in v09_00_00?
Best Regards,
Mathias