This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: Build error #10010 using GPIO test project

Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAPL138

Tool/software:

Hello,

I wanted to use the sample project “GPIO_LedBlink_lcdkOMAPL138_c674xTestProject”, but I get the following error:


[0]**** Build of configuration Debug for project GPIO_LedBlink_lcdkOMAPL138_c674xTestProject ****
[1]"C:\\ti\\ccs2001\\ccs\\utils\\bin\\gmake" -k -j 12 all -O 
 
[2]Building target: "GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.out"
[3]Invoking: C6000 Linker
[4]"C:/ti/ti-cgt-c6000_8.5.0.LTS/bin/cl6x" -mv6740 --define=SOC_OMAPL138 --define=LCDK_OMAPL138 --define=USE_BIOS --define=lcdkOMAPL138 --define=c6748 -g --diag_suppress=1111 --diag_suppress=827 --diag_suppress=824 --diag_suppress=837 --diag_suppress=1037 --diag_suppress=195 --diag_suppress=77 --diag_suppress=232 --diag_warning=225 --diag_warning=994 --diag_warning=262 --diag_wrap=off --display_error_number -z -m"GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ti-cgt-c6000_8.5.0.LTS/lib" -i"C:/ti/ti-cgt-c6000_8.5.0.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="GPIO_LedBlink_lcdkOMAPL138_c674xTestProject_linkInfo.xml" --ram_model -o "GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.out" "./GPIO_board.obj" "./main_led_blink.obj" "../C6748.cmd" -l"configPkg/linker.cmd"  -llibc.a 
[5]<Linking>
[6]"configPkg/linker.cmd", line 34: error #10264: L3_CBA_RAM memory range overlaps existing memory range SHRAM
[7]error #10010: errors encountered during linking; "GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.out" not built
 
[8]>> Compilation failure
[9]gmake[1]: *** [makefile:138: GPIO_LedBlink_lcdkOMAPL138_c674xTestProject.out] Error 1
[10]gmake: *** [makefile:132: all] Error 2
[11]**** Build Finished ****