AM625: u-boot failed to initialize 8Gb of DDR4 with sysconfig configuration

Part Number: AM625
Other Parts Discussed in Thread: SYSCONFIG,

Tool/software:

Hello,

I got the last version of our custom design base on AM265 with 2x32Gbits DDR4 chip (Micron MT40A4G8NEA-062E:F) connected to CS0 and CS1.

I use the DDR sysconfig tools to generate the configuration, the file is joined: 

Data Bus Width (per device) 8
Density (per device) (Gb) 32
Chip Selects / Ranks 2

The default memory mapping device tree configuration is:

k3-am625-sk.dts
        memory@80000000 {
                device_type = "memory";
               /* 4G RAM */
               reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
                       <0x00000008 0x80000000 0x00000000 0x80000000>;

        };

k3-am62x-sk-common.dtsi
        memory@80000000 {
                bootph-pre-ram;
                device_type = "memory";
               /* 4G RAM */
               reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
                       <0x00000008 0x80000000 0x00000000 0x80000000>;
        };


The 8GB memory mapping device tree configuration is:

k3-am625-sk.dts
        memory@80000000 {
                device_type = "memory";
               /* 8G RAM */
               reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
                       <0x00000008 0x80000000 0x00000001 0x80000000>;

        };

k3-am62x-sk-common.dtsi
        memory@80000000 {
                bootph-pre-ram;
                device_type = "memory";
               /* 8G RAM */
               reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
                       <0x00000008 0x80000000 0x00000001 0x80000000>;
        };

The bank 0 size is 2GBytes, and the bank 1 size is 6GBytes.

I don't know 

This configuration is correctly handle by the u-boot command bdinfo.

=> bdinfo
boot_params = 0x0000000000000000
DRAM bank = 0x0000000000000000
-> start = 0x0000000080000000
-> size = 0x0000000080000000
DRAM bank = 0x0000000000000001
-> start = 0x0000000880000000
-> size = 0x0000000180000000
flashstart = 0x0000000000000000
flashsize = 0x0000000000000000
flashoffset = 0x0000000000000000
baudrate = 115200 bps
relocaddr = 0x00000000fff03000
reloc off = 0x000000007f703000
Build = 64-bit
current eth = ethernet@8000000port@1
ethaddr = 28:b5:e8:d4:64:6b
IP addr = 10.0.0.5
fdt_blob = 0x00000000fded0670
new_fdt = 0x00000000fded0670
fdt_size = 0x0000000000013700
multi_dtb_fit= 0x0000000000000000
lmb_dump_all:
memory.cnt = 0x2 / max = 0x10
memory[0] [0x80000000-0xffffffff], 0x80000000 bytes flags: 0
memory[1] [0x880000000-0x9ffffffff], 0x180000000 bytes flags: 0
reserved.cnt = 0x6 / max = 0x10
reserved[0] [0x9c700000-0x9c7fffff], 0x00100000 bytes flags: 0
reserved[1] [0x9c800000-0x9d9fffff], 0x01200000 bytes flags: 4
reserved[2] [0x9db00000-0x9e6fffff], 0x00c00000 bytes flags: 4
reserved[3] [0x9e780000-0x9fffffff], 0x01880000 bytes flags: 4
reserved[4] [0xfcec3000-0xffffffff], 0x0313d000 bytes flags: 0
reserved[5] [0x880000000-0x9ffffffff], 0x180000000 bytes flags: 0
devicetree = separate
serial addr = 0x0000000002800000
width = 0x0000000000000000
shift = 0x0000000000000002
offset = 0x0000000000000000
clock = 0x0000000002dc6c00
stack ptr = 0x00000000fdecf9f8
ram_top ptr = 0x0000000100000000
malloc base = 0x00000000fdee4000
arch_number = 0x0000000000000000
TLB addr = 0x00000000ffff0000
irq_sp = 0x00000000fdecfff0
sp start = 0x00000000fdecfff0
Early malloc usage: 3bc0 / 8000

But the command meminfo doesn't indicates the correct value : 

=> meminfo
DRAM:  2 GiB

The memory access failed over the 2GBytes in bank1: 

=> mw.b 0x900000000 55
"Synchronous Abort" handler, esr 0x96000045, far 0x900000000
elr: 000000008081daa4 lr : 000000008081da24 (reloc)
elr: 00000000fff20aa4 lr : 00000000fff20a24
x0 : 0000000000000000 x1 : 0000000900000000
x2 : 0000000000000001 x3 : 00000000fdf03df2
x4 : 0000000000000100 x5 : 0000000000000000
x6 : 00000000fffb00ad x7 : 0000000000000044
x8 : 0000000000000010 x9 : 0000000000000005
x10: 0000000000000006 x11: 000000000001869f
x12: 00000000ffffffff x13: 0000000100000000
x14: 00000000ffffffff x15: 00000000fdecf848
x16: 00000000fff209bc x17: 0000000000000000
x18: 00000000fdee3d70 x19: 0000000900000000
x20: 0000000000000001 x21: 0000000000000055
x22: 00000000fdefc650 x23: 0000000000000003
x24: 00000000fffea840 x25: 0000000000000000
x26: 0000000000000000 x27: 0000000000000000
x28: 00000000fdf03e10 x29: 00000000fdecfcf0

Code: 71000a9f 54000061 79000035 17fffff7 (39000035)
Resetting CPU ...

resetting ...

Could you help us to identify fix the issue.

 k3-am62x-ddr-config-8-32-2.txt

  • Alexis, let me double check with the software team on the device tree changes.

    In the meantime, can you try with:

    Data Bus Width (per device) 8
    Density (per device) (Gb) 16
    Chip Selects / Ranks 2

    Regards,

    James

  • Hello James,

    Here are the information return by u-boot with the configuration: 

    Data Bus Width (per device) 8
    Density (per device) (Gb) 16
    Chip Selects / Ranks 2

    => bdinfo
    boot_params = 0x0000000000000000
    DRAM bank   = 0x0000000000000000
    -> start    = 0x0000000080000000
    -> size     = 0x0000000080000000
    DRAM bank   = 0x0000000000000001
    -> start    = 0x0000000880000000
    -> size     = 0x0000000080000000
    flashstart  = 0x0000000000000000
    flashsize   = 0x0000000000000000
    flashoffset = 0x0000000000000000
    baudrate    = 115200 bps
    relocaddr   = 0x00000000fff03000
    reloc off   = 0x000000007f703000
    Build       = 64-bit
    current eth = ethernet@8000000port@1
    ethaddr     = 28:b5:e8:d4:64:6b
    IP addr     = 10.0.0.5
    fdt_blob    = 0x00000000fded0670
    new_fdt     = 0x00000000fded0670
    fdt_size    = 0x0000000000013700
    multi_dtb_fit= 0x0000000000000000
    lmb_dump_all:
     memory.cnt = 0x2 / max = 0x10
     memory[0]      [0x80000000-0xffffffff], 0x80000000 bytes flags: 0
     memory[1]      [0x880000000-0x8ffffffff], 0x80000000 bytes flags: 0
     reserved.cnt = 0x6 / max = 0x10
     reserved[0]    [0x9c700000-0x9c7fffff], 0x00100000 bytes flags: 0
     reserved[1]    [0x9c800000-0x9d9fffff], 0x01200000 bytes flags: 4
     reserved[2]    [0x9db00000-0x9e6fffff], 0x00c00000 bytes flags: 4
     reserved[3]    [0x9e780000-0x9fffffff], 0x01880000 bytes flags: 4
     reserved[4]    [0xfcec7000-0xffffffff], 0x03139000 bytes flags: 0
     reserved[5]    [0x880000000-0x8ffffffff], 0x80000000 bytes flags: 0
    devicetree  = separate
    serial addr = 0x0000000002800000
     width      = 0x0000000000000000
     shift      = 0x0000000000000002
     offset     = 0x0000000000000000
     clock      = 0x0000000002dc6c00
    stack ptr   = 0x00000000fdecf9f8
    ram_top ptr = 0x0000000100000000
    malloc base = 0x00000000fdee4000
    arch_number = 0x0000000000000000
    TLB addr    = 0x00000000ffff0000
    irq_sp      = 0x00000000fdecfff0
    sp start    = 0x00000000fdecfff0
    Early malloc usage: 3bc0 / 8000

    I use the device tree file generated by the tool DDR sysconfig for the AM625.

    There is no error accessing the no reserve memory in bank 0 and bank 1.

    Regards,

    Alexis.

  • Hi Alexis, so are you able to uniquely access the full 8GByte range?

    Regards,

    James

  • Hi James, I'm not sure to understand what you mean by "full 8GBytes range". I can only access 4GB of memory.

    I mean 2GBytes on bank0 and 2GBytes on bank1, it is what I program in the memory section in the device tree for the test with the last configuration you asked me to test. If I'm right a density of 16Gbits with 2 ranks is for a total of 4GBytes of memory. Is it exact ?

    So no I don't have access to the full range, only 4GB over 8GB.

    Regards,

    Alexis.

  • Hi Alexis,

    we believe there is some limitation in the addressing in uboot.  We are still investigating this.

    In the meantime, if you go back to:

    Data Bus Width (per device) 8
    Density (per device) (Gb) 32
    Chip Selects / Ranks 2

    are you able to boot into the kernel?  If so, can you try to access bank1 above 0x900000000?

    Also, what version of SDK are you using?

    Regards,

    James

  • Hi James,

    1 - Also, what version of SDK are you using?

    I use SDK 10 with ti-u-boot version 10.00.07 and ti-kernel-linux version 10.00.07.

    2 - are you able to boot into the kernel? 

    Yes, but with 4Gb configured, I can't boot with 8Gb configured.

    I will do the test again to capture kernel log.

    3 - If so, can you try to access bank1 above 0x900000000?

    I configure 8Gb with Databus width 8, Density 32 and rank2.

    The access from u-boot to address  0x900000000 and higher leads to a reset of the board:

    As I mentioned the u-boot memory mapping is: 

    DRAM bank = 0x0000000000000000
    -> start = 0x0000000080000000
    -> size = 0x0000000080000000
    DRAM bank = 0x0000000000000001
    -> start = 0x0000000880000000
    -> size = 0x0000000180000000

    => mw.b 0x900000000 55
    "Synchronous Abort" handler, esr 0x96000045, far 0x900000000
    elr: 000000008081daa4 lr : 000000008081da24 (reloc)
    elr: 00000000fff20aa4 lr : 00000000fff20a24
    x0 : 0000000000000000 x1 : 0000000900000000
    x2 : 0000000000000001 x3 : 00000000fdf03df2
    x4 : 0000000000000100 x5 : 0000000000000000
    x6 : 00000000fffb00ad x7 : 0000000000000044
    x8 : 0000000000000010 x9 : 0000000000000005
    x10: 0000000000000006 x11: 000000000001869f
    x12: 00000000ffffffff x13: 0000000100000000
    x14: 00000000ffffffff x15: 00000000fdecf848
    x16: 00000000fff209bc x17: 0000000000000000
    x18: 00000000fdee3d70 x19: 0000000900000000
    x20: 0000000000000001 x21: 0000000000000055
    x22: 00000000fdefc650 x23: 0000000000000003
    x24: 00000000fffea840 x25: 0000000000000000
    x26: 0000000000000000 x27: 0000000000000000
    x28: 00000000fdf03e10 x29: 00000000fdecfcf0

    Code: 71000a9f 54000061 79000035 17fffff7 (39000035)
    Resetting CPU ...

    Regards,

    Alexis

  • Hi Alexis,

    we are able to reproduce this issue, and it is a limitation in u-boot as the higher addresses are not mapped. Since u-boot does not use more than 4GBytes, it was never mapped in earlier SDKs.  So when you try to write into those higher banks, it will crash

    If you use SDK11, this issue is fixed, and you would be able to access the higher banks in u-boot using those commands.

    However, if you are still using SDK10, you won't be able to access the higher banks in u-boot (ie, the aborts you are seeing is expected), but you should still be able to boot into the kernel using 8GB, and then you should be able to access the full 8GB range from the kernel prompt.

    Please provide full boot log with 8GB configured.  Ensure DDR config uses:

    Data Bus Width (per device) 8
    Density (per device) (Gb) 32
    Chip Selects / Ranks 2

    Regards,

    James

  • Hi James,

    I tried to apply my patch from TiSDK10 to the u-boot version used by the TiSDK11, but some files are missing and memory is no more present in the device tree.

    The use the information from the TiSDK11 to build u-boot from source: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/11_01_05_03/exports/docs/linux/Foundational_Components/U-Boot/BG-Build-K3.html#build-u-boot.

    Could you give me which files must be modified to configure u-boot to use 8Gb of memory.

    Regards,

    Alexis.

  • Hi Alexis,

    Since U-Boot v2025.01 which is used on SDK11.x, the devicetree files have been moved from <U-Boot>/arch/arm/dts/ directory to <U-Boot>/dts/upstream/src/arm64/ti/ to align with the devicetree files in kernel. But the U-Boot specific devicetree files (for example, DDR config) are still in the original directory.

    If you still have problem in moving to SDK11 U-Boot, please provide your SDK10 U-Boot patch or list which files have been modified, I can show you which corresponding files to be modified in SDK11 U-Boot.

  • Hi Bin,

    Thanks for your help.

    Here are the file I modified in u-boot to configure for 4GB of DDR4, with 1 rank.

    But I need to modify the memory configuration for 8GB of DDR4, let me know which file must be modified.

    - I replace the DDR4 configuration by the sysconfig file with Bus width 8 bits, Density 32Gb and rank 2
    The file is arch/arm/dts/k3-am62x-sk-ddr4-1600MTs.dtsi

    - Then I modify memory node to have 2 banks of memory for 4GB, it must be change to 8GB.

    diff --git a/arch/arm/dts/k3-am625-sk.dts b/arch/arm/dts/k3-am625-sk.dts
    index 5ca722aec43..c8f9cd05fe7 100644
    --- a/arch/arm/dts/k3-am625-sk.dts
    +++ b/arch/arm/dts/k3-am625-sk.dts
    @@ -24,8 +24,9 @@

            memory@80000000 {
                    device_type = "memory";
    -               /* 2G RAM */
    -               reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
    +               /* 4G RAM */
    +               reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
    +                       <0x00000008 0x80000000 0x00000000 0x80000000>;

            };

    - Same thing that above.


    diff --git a/arch/arm/dts/k3-am62x-sk-common.dtsi b/arch/arm/dts/k3-am62x-sk-common.dtsi
    index 59ee4961650..fb5f85cda42 100644
    --- a/arch/arm/dts/k3-am62x-sk-common.dtsi
    +++ b/arch/arm/dts/k3-am62x-sk-common.dtsi
    @@ -30,8 +30,9 @@
            memory@80000000 {
                    bootph-pre-ram;
                    device_type = "memory";
    -               /* 2G RAM */
    -               reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
    +               /* 4G RAM */
    +               reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
    +                       <0x00000008 0x80000000 0x00000000 0x80000000>;
            };

    - I disabled CONFIG_ARCH_FIXUP_FDT_MEMORY in u-boot to use the memory mapping define in the linux kernel device tree.

    I don't know if it is still necessary, let me know if I have to remove this patch.


    +++ b/configs/am62x_evm_a53_defconfig
    @@ -35,6 +35,7 @@ CONFIG_SPL_LOAD_FIT_ADDRESS=0x81000000
     CONFIG_BOOTSTD_FULL=y
     CONFIG_OF_BOARD_SETUP=y
     CONFIG_FDT_SIMPLEFB=y
    +# CONFIG_ARCH_FIXUP_FDT_MEMORY is not set
     CONFIG_BOARD_LATE_INIT=y
     CONFIG_BLOBLIST=y
     CONFIG_BLOBLIST_ADDR=0x80D00000

    Regards,

    Alexis.

  • Hi Alexis,

    But I need to modify the memory configuration for 8GB of DDR4, let me know which file must be modified.

    For SDK10.x, it will still be in the same file: arch/arm/dts/k3-am625-sk.dts.

    +++ b/arch/arm/dts/k3-am625-sk.dts
    @@ -24,8 +24,9 @@

            memory@80000000 {
                    device_type = "memory";
    -               /* 2G RAM */
    -               reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
    +               /* 4G RAM */
    +               reg = <0x00000000 0x80000000 0x00000000 0x80000000>,
    +                       <0x00000008 0x80000000 0x00000000 0x80000000>;

    In each line of the 'reg' property of memory@800000000 node, the first two numbers are the DDR address (64bit), the last two numbers are the DDR size (64bit). So change the last two numbers at following for 8 GB DDR.

    <0x00000008 0x80000000 0x00000001 0x80000000>;

    - Same thing that above.


    diff --git a/arch/arm/dts/k3-am62x-sk-common.dtsi b/arch/arm/dts/k3-am62x-sk-common.dtsi

    You don't need to modify the same in k3-am62x-sk-common.dtsi. This file is included in k3-am625-sk.dts, so the memory setting is overwritten by those in k3-am625-sk.dts.

    FYI, the memory@80000000 node in k3-am62x-sk-common.dtsi has been removed in the latest devicetree code, since it is redundant.

    - I disabled CONFIG_ARCH_FIXUP_FDT_MEMORY in u-boot to use the memory mapping define in the linux kernel device tree.

    I don't know if it is still necessary, let me know if I have to remove this patch.

    No, you shouldn't disable it. it would cause kernel boot to stop.

  • For SDK10.x, it will still be in the same file: arch/arm/dts/k3-am625-sk.dts.

    Forgot to mention, this file has been moved to <U-Boot>/dts/upstream/src/arm64/ti/ directory in SDK11.x U-Boot.

  • Hi Bin,

    I look at the TI u-boot repo at tag 11.01.05: https://git.ti.com/cgit/ti-u-boot/ti-u-boot/tree/arch/arm/dts?h=11.01.05.

    There is no more the file k3-am625-sk.dts.

    There is a file k3-am625-r5-sk.dts, do I need to path it also ?

    By the way I modify the following files, to check that my modifications are applied.

    I configure the 2 banks and reduced the first bank from 2GB to 1GB.

    I can see that the modification of the first memory bank is done, but there is not the second bank.

     Here is the u-boot logs:

    -Boot 2025.01-00531-g1ac7b41e843c (Oct 02 2025 - 17:18:59 +0200)

    SoC:   AM62X SR1.0 HS-FS
    Model: Texas Instruments AM625 SK
    DRAM:  1 GiB
    Core:  83 devices, 32 uclasses, devicetree: separate
    MMC:   mmc@fa10000: 0, mmc@fa00000: 1
    Loading Environment from nowhere... OK
    In:    serial
    Out:   serial
    Err:   serial
    Net:   eth0: ethernet@8000000port@1

    Hit any key to stop autoboot:  0 
    => bdinfo
    boot_params = 0x0000000000000000
    DRAM bank   = 0x0000000000000000
    -> start    = 0x0000000080000000
    -> size     = 0x0000000040000000
    flashstart  = 0x0000000000000000
    flashsize   = 0x0000000000000000
    flashoffset = 0x0000000000000000
    baudrate    = 115200 bps
    relocaddr   = 0x00000000bfe9a000
    reloc off   = 0x000000003f69a000

    Could you confirm that the second bank is well managed by the SDK11 ?

    Here are the patches.

    diff --git a/arch/arm/dts/k3-am62-sk-common-u-boot.dtsi b/arch/arm/dts/k3-am62-sk-common-u-boot.dtsi
    index b88c1fb6191..9b153eaf044 100644
    --- a/arch/arm/dts/k3-am62-sk-common-u-boot.dtsi
    +++ b/arch/arm/dts/k3-am62-sk-common-u-boot.dtsi
    @@ -11,6 +11,14 @@
             tick-timer = &main_timer0;
         };
     
    +        memory@80000000 {
    +                device_type = "memory";
    +                /* 8G RAM */
    +                reg = <0x00000000 0x80000000 0x00000000 0x40000000>,
    +                      <0x00000008 0x80000000 0x00000001 0x80000000>;
    +                bootph-pre-ram;
    +        };
    +
         panel_lvds: panel-lvds {
             bootph-pre-ram;
             compatible = "simple-panel";
    -- 
    2.34.1

    diff --git a/dts/upstream/src/arm64/ti/k3-am625-sk.dts b/dts/upstream/src/arm64/ti/k3-am625-sk.dts
    index 6cd74660292..b5c51789eb5 100644
    --- a/dts/upstream/src/arm64/ti/k3-am625-sk.dts
    +++ b/dts/upstream/src/arm64/ti/k3-am625-sk.dts
    @@ -28,8 +28,9 @@
            memory@80000000 {
                    bootph-pre-ram;
                    device_type = "memory";
    -               /* 2G RAM */
    -               reg = <0x00000000 0x80000000 0x00000000 0x80000000>;
    +               /* 8G RAM */
    +               reg = <0x00000000 0x80000000 0x00000000 0x40000000>,
    +                     <0x00000008 0x80000000 0x00000001 0x80000000>;

            };

    Regards,

    Alexis.

  • Hello,

    Without any response I made a diff between the u-boot configuration of the SDK10 and SDK11. I saw that one developer commit a change regarding the number of memory bank supported by the AM625. Could you clarify why such modification has been made ?

    Could you also indicated the best way to validate the 8GB of memory under Linux, does I need to modify something to make the memory test tools memtest or stress-ng working ?

    Regards,

    Alexis.

  • Alexis, best way to validate 8GB in linux is to first perform a sanity check that you can *uniquely* write to the whole memory:

    Use devmem2 tool from linux prompt to perform single writes of unique values across the memory (eg, at 0x80000000, 0xC0000000, 0x880000000, 0x900000000, 0x980000000, etc) . Then perform a readback of those same locations to ensure values are correct and were not overwritten due to aliasing.

    The linux memtester tool will stress the interface, it is not necessary to test specific addresses.  But if you want linux to choose an address from a certain region, i believe you can modify the DT to reserve this memory region first, then you can run memtester on it.  Bin should be able to give more details on this.

    Regards,

    James

  • Hello James,

    I have done some tests I reserved the area 880000000-9ffffffff as shown below: 

    80080000-9c7fffff : System RAM
      82010000-830effff : Kernel code
      830f0000-8338ffff : reserved
      83390000-8357ffff : Kernel data
      87fff000-87ffffff : reserved
      8ffee000-8fffcfff : reserved
      9c700000-9c7fffff : reserved
    9c800000-9e6fffff : reserved
    9e700000-9e7fffff : System RAM
    9e800000-9fffffff : reserved
    a0000000-ffffffff : System RAM
      eb740000-f79fffff : reserved
      f7a6d000-f7b6dfff : reserved
      f7b6e000-f7bc5fff : reserved
      f7bc8000-f7bc8fff : reserved
      f7bc9000-f7bcbfff : reserved
      f7bcc000-f7bddfff : reserved
      f7bde000-ffffffff : reserved
    500000000-5ffffffff : fc40000.spi spi@fc40000
    880000000-9ffffffff : reserved

    I compile devmem2 to access several address between 0x880000000 0x9FFFFFFFF, and the R/W access works.

    So I clone the code and add a feature to write a range of address.

    - For the range 0x880000000 for a size of 80000000 (2GB) there is no errors.

    - For the range 0x900000000 for a size of 80000000 (2GB) the Linux kernel hang, if the first area 16 Mo.

    I done several test with tisdk11 with the yocto build and the armbian trixie distribution.

    The results are the same, the test shown that the kernel crash at differents offset.

    By example:

    0x900000000 + 0x2347d0

    0x900000000 + 0x17c338

    0x910000000 + 0x22a76d 

    I also do a test stress for the CPU without any issue, and done the same test with only 1 cpu enable, but the issue is still there.

    Could you help us to identify the issue ?

    Do you think I can modify some parameter with the DDR sysconfig tools, to isolate the root cause of the probleme ?

    Do you have any JTAG script that can help to test the DDR without Linux running ?

    Regards,

    Alexis.

  • Hi Alexis,

    What is the output of the following command on your board right after boot into linux?

    # dmesg | grep 'Memory:'

  • Hi Bin,

    Here is the ouput of 'dmesg | grep 'Memory:'':

    Memory: 1672660K/8388608K available (12992K kernel code, 1256K rwdata, 4668K rodata, 2752K init, 642K bss, 6576964K reserved, 131072K cma-reserved)

    I add the output of:

    - cat /proc/meminfo
    MemTotal: 1814396 kB
    MemFree: 1525008 kB
    MemAvailable: 1562488 kB
    Buffers: 1052 kB
    Cached: 162932 kB
    SwapCached: 0 kB
    Active: 24328 kB
    Inactive: 193904 kB
    Active(anon): 780 kB
    Inactive(anon): 62724 kB
    Active(file): 23548 kB
    Inactive(file): 131180 kB
    Unevictable: 0 kB
    Mlocked: 0 kB
    SwapTotal: 0 kB
    SwapFree: 0 kB
    Dirty: 0 kB
    Writeback: 0 kB
    AnonPages: 54248 kB
    Mapped: 73888 kB
    Shmem: 9256 kB
    KReclaimable: 13568 kB
    Slab: 32932 kB
    SReclaimable: 13568 kB
    SUnreclaim: 19364 kB
    KernelStack: 2316 kB
    PageTables: 2472 kB
    SecPageTables: 0 kB
    NFS_Unstable: 0 kB
    Bounce: 0 kB
    WritebackTmp: 0 kB
    CommitLimit: 907196 kB
    Committed_AS: 315344 kB
    VmallocTotal: 135288315904 kB
    VmallocUsed: 11188 kB
    VmallocChunk: 0 kB
    Percpu: 1024 kB
    HardwareCorrupted: 0 kB
    AnonHugePages: 14336 kB
    ShmemHugePages: 0 kB
    ShmemPmdMapped: 0 kB
    FileHugePages: 0 kB
    FilePmdMapped: 0 kB
    CmaTotal: 131072 kB
    CmaFree: 129584 kB
    HugePages_Total: 0
    HugePages_Free: 0
    HugePages_Rsvd: 0
    HugePages_Surp: 0
    Hugepagesize: 2048 kB
    Hugetlb: 0 kB

    - cat /proc/iomem
    000f4000-000f42ab : pinctrl-single
    00104044-0010404b : 104044.phy phy@4044
    00600000-006000ff : 600000.gpio gpio@600000
    00601000-006010ff : 601000.gpio gpio@601000
    00b00000-00b003ff : b00000.temperature-sensor temperature-sensor@b00000
    00b01000-00b013ff : b00000.temperature-sensor temperature-sensor@b00000
    01800000-0180ffff : GICD
    01880000-0193ffff : GICR
    02400000-024003ff : 2400000.timer timer@2400000
    02410000-024103ff : 2410000.timer timer@2410000
    02420000-024203ff : 2420000.timer timer@2420000
    02430000-024303ff : 2430000.timer timer@2430000
    02440000-024403ff : 2440000.timer timer@2440000
    02450000-024503ff : 2450000.timer timer@2450000
    02460000-024603ff : 2460000.timer timer@2460000
    02470000-024703ff : 2470000.timer timer@2470000
    02800000-0280001f : serial
    04084000-04084087 : pinctrl-single
    05000000-0502ffff : 5000000.m4fss
    05040000-0504ffff : 5000000.m4fss
    08000000-081fffff : 8000000.ethernet cpsw_nuss
    0e000000-0e0000ff : e000000.watchdog watchdog@e000000
    0e010000-0e0100ff : e010000.watchdog watchdog@e010000
    0e020000-0e0200ff : e020000.watchdog watchdog@e020000
    0e030000-0e0300ff : e030000.watchdog watchdog@e030000
    0e0f0000-0e0f00ff : e0f0000.watchdog watchdog@e0f0000
    0f900000-0f9007ff : f900000.dwc3-usb dwc3-usb@f900000
    0f908000-0f9083ff : f900000.dwc3-usb dwc3-usb@f900000
    0f910000-0f9107ff : f910000.dwc3-usb dwc3-usb@f910000
    0f918000-0f9183ff : f910000.dwc3-usb dwc3-usb@f910000
    0fa10000-0fa10fff : fa10000.mmc mmc@fa10000
    0fa18000-0fa183ff : fa10000.mmc mmc@fa10000
    0fc40000-0fc400ff : fc40000.spi spi@fc40000
    20000000-200000ff : 20000000.i2c i2c@20000000
    20010000-200100ff : 20010000.i2c i2c@20010000
    20020000-200200ff : 20020000.i2c i2c@20020000
    29000000-290001ff : 29000000.mailbox mailbox@29000000
    2a000000-2a000fff : 2a000000.spinlock spinlock@2a000000
    2b1f0000-2b1f00ff : 2b1f0000.rtc rtc@2b1f0000
    30300000-30300fff : 30300000.crc crc@30300000
    3100c100-3104ffff : 31000000.usb usb@31000000
    31100000-31107fff : usb@31100000
    31100000-31107fff : xhci-hcd.0.auto usb@31100000
    3110c100-3114ffff : 31100000.usb usb@31100000
    40900000-409011ff : 40900000.crypto crypto@40900000
    43000014-43000017 : 43000014.chipid chipid@14
    44043000-44043fdf : 44043000.system-controller debug_messages
    48000000-480fffff : 48000000.interrupt-controller interrupt-controller@48000000
    485c0000-485c00ff : 485c0000.dma-controller gcfg
    485c0100-485c01ff : 485c0100.dma-controller gcfg
    4a400000-4a47ffff : 4d000000.mailbox scfg
    4a600000-4a67ffff : 4d000000.mailbox rt
    4a800000-4a81ffff : 485c0000.dma-controller rchanrt
    4a820000-4a83ffff : 485c0100.dma-controller rchanrt
    4aa00000-4aa1ffff : 485c0000.dma-controller tchanrt
    4aa40000-4aa5ffff : 485c0100.dma-controller tchanrt
    4b800000-4b9fffff : 485c0000.dma-controller ringrt
    4bc00000-4bcfffff : 485c0100.dma-controller ringrt
    4c000000-4c01ffff : 485c0100.dma-controller bchanrt
    4d000000-4d07ffff : 4d000000.mailbox target_data
    70000000-7000ffff : 70000000.sram sram@70000000
    78000000-78007fff : 78000000.r5f
    78100000-78107fff : 78000000.r5f
    80000000-8007ffff : reserved
    80080000-9c7fffff : System RAM
    82010000-8315ffff : Kernel code
    83160000-8340ffff : reserved
    83410000-835fffff : Kernel data
    87fff000-87ffffff : reserved
    8ffee000-8fffcfff : reserved
    9c700000-9c7fffff : reserved
    9c800000-9e6fffff : reserved
    9e700000-9e7fffff : System RAM
    9e800000-9fffffff : reserved
    a0000000-ffffffff : System RAM
    eb740000-f79fffff : reserved
    f7a6d000-f7b6dfff : reserved
    f7b6e000-f7bc5fff : reserved
    f7bc8000-f7bc8fff : reserved
    f7bc9000-f7bcbfff : reserved
    f7bcc000-f7bddfff : reserved
    f7bde000-ffffffff : reserved
    500000000-5ffffffff : fc40000.spi spi@fc40000
    880000000-9ffffffff : reserved

    Regards,

    Alexis.

  • Hi Alexis, sorry, some of your answers are unclear to me, can you clarify:

    I compile devmem2 to access several address between 0x880000000 0x9FFFFFFFF, and the R/W access works.

    Does this mean you tried several read/write across all of 0x880000000 thru 0x9FFFFFFFF successfully using devmem2?  Did you ensure that you can uniquely access this region of memory (ie, writing to 0x880000000 doesn't affect 0x900000000 or 0x980000000, for example)?

    So I clone the code and add a feature to write a range of address.

    - For the range 0x880000000 for a size of 80000000 (2GB) there is no errors.

    - For the range 0x900000000 for a size of 80000000 (2GB) the Linux kernel hang, if the first area 16 Mo.

    What do you mean by "if the first area 16 Mo."?  

    I done several test with tisdk11 with the yocto build and the armbian trixie distribution.

    The results are the same, the test shown that the kernel crash at differents offset.

    By example:

    0x900000000 + 0x2347d0

    0x900000000 + 0x17c338

    0x910000000 + 0x22a76d 

    Can you explain this test, or better yet, post this log?  When you write the range of addresses, does it work for a while and then fail at one of those offsets?  Or were you able to write the whole block successfully and only failed at those 3 offsets?

    I also do a test stress for the CPU without any issue

    What stress test did you run?  This indicates that you have a robust DDR configuration

    and done the same test with only 1 cpu enable, but the issue is still there.

    I don't understand this.  Was the stress test that was successful run with multiple CPUs?

    If i'm interpreting your answers correctly, it looks like you can successfully access all 8GB of memory, and you have run a stress test and passed.  So i'm not sure why you are still seeing hang issues.

    Regards,

    James

  • Hi James,

    The memory tests over the 8 GB of RAM are successful, they run for more that 5 hours without error. The configuration is now integrated and deployed on our prototype.

    Thank you very much.

    Alexis.

  • Hi Alexis, this is great to hear!!  Do you know what the ultimate root cause was?

    Regards,

    James