Tool/software: AM62A processor SDK v11.01.07.05
I'm having a problem with the tiovxmultiscaler gstreamer plugin - this is how I have it setup
Tool/software: AM62A processor SDK v11.01.07.05
I'm having a problem with the tiovxmultiscaler gstreamer plugin - this is how I have it setup
Hello Michael,
We have recently discovered that the following PRs were problematic and may be the root cause for the symptom you're seeing:
https://github.com/TexasInstruments/edgeai-gst-plugins/pull/368/files
https://github.com/TexasInstruments/edgeai-tiovx-modules/pull/90/files
Would you please try to remove these changes and rebuild edgeai-tiovx-modules and edgeai-gst-plugins? See if that helps.
Regards,
Jianzhong
Hi Jianzhong Xu ,
For edgeai-tiovx-modules that PR doesn't revert cleanly from the top of 11.01.07.05 (commit 16ea980baf...), there are some conflicts.
I've tried a few different iterations removing input_params and crop_params from edgeai-gst-plugins + edgeai-tiovx-modules but no luck, I either get the same result or a crash.
Could you please try to replicate on your side? Seems to me that ROI doesn't work at all. I am just using v11.01.07.05 out of the box.
Cheers,
Michael
My mistake Jianzhong Xu  - seems like I foolishly renamed pad 'src_0' to 'src' in my debugging and that invalidated the fix.
I can confirm that just reverting https://github.com/TexasInstruments/edgeai-gst-plugins/pull/368/files solved my issue! 
This command works as expected now: