Tool/software:
Hello TI Team,
I’m working with the T3 Gemstone O1 (AM67A-based) board and trying to perform DFU (Device Firmware Upgrade) boot.
When I use the tiboot3.bin and tispl.bin from the official TI Processor SDK (09_02_00_05) along with my custom-built u-boot.img (from my own Yocto-based SDK), the DFU process works perfectly:
* DFU communication is established
* Files are transferred successfully
* Boot sequence proceeds normally