Hello:
I can not used the eth during falcon mode:
Here is the step of falcon mode i have follow:
It seems that the driver have be add but the eth was not register
here is the whole log file: log.txt
root@am62axx-evm:/opt/edgeai-gst-apps# ifconfig
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 16 bytes 2112 (2.0 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 16 bytes 2112 (2.0 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# ip addr add 172.16.1.1/24 dev eth0
Cannot find device "eth0"
root@am62axx-evm:/opt/edgeai-gst-apps#