Part Number: TMDSCNCD263P
Other Parts Discussed in Thread: SYSCONFIG,
Hi,
I am working on getting FSI working on the AM263 control card. I have a very simple program running, which simply sends a ping frame and receives it:
/* send ping frame*/ status = FSI_setTxFrameType(txBaseAddr, FSI_FRAME_TYPE_PING); status += FSI_setTxFrameTag(txBaseAddr, FSI_FRAME_TAG1); status += FSI_startTxTransmit(txBaseAddr); status += SemaphoreP_pend(&gFsiTxSemObject, ClockP_usecToTicks(FSI_TX_TIMEOUT_US)); if(status != SystemP_SUCCESS) { DebugP_log("failed to send ping frame\r\n"); continue; } DebugP_log("sent ping frame\r\n"); /* receive ping frame*/ status += SemaphoreP_pend(&gFsiRxSemObject, ClockP_usecToTicks(FSI_RX_TIMEOUT_US)); status += FSI_getRxFrameType(rxBaseAddr, &frameType); status += FSI_getRxPingTag(rxBaseAddr, &rxFrameTag); if (status != SystemP_SUCCESS) { DebugP_log("failed to receive ping frame\r\n"); continue; } DebugP_log("received ping frame: frame tag = %u\r\n", rxFrameTag);The MCAN signals go through a 1:2 signal routing mux. There is a pull-down resistor on the select line of the mux and therefore the MCAN signal routing is the default.
| FSIRX2_CLK | J2 |
| FSIRX2_DATA0 | G4 |
| FSIRX2_DATA1 | J3 |
| FSITX2_CLK | G3 |
| FSITX2_DATA0 | H2 |
| FSITX2_DATA1 | G1 |


Thanks,