This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62L: DDR RAM optimization

Part Number: AM62L

Hii, 

As per the TI_Thread DDR optimization changes I done all things.

But board is not booting after below logs:

NOTICE:  bl1_plat_arch_setup arch setup
NOTICE:  Booting Trusted Firmware
NOTICE:  BL1: v2.12.0(release):11.00.15-dirty
NOTICE:  BL1: Built : 12:24:23, May 29 2025
NOTICE:  BL1: dram_class: 11
NOTICE:  lpddr4: post start - PI training status=0x27c0a000
NOTICE:  bl1_platform_setup DDR init done
NOTICE:  k3_bl1_handoff ENTERING WFI - end of bl1
NOTICE:  BL31: v2.12.0(release):11.00.15-dirty
NOTICE:  BL31: Built : 12:24:23, May 29 2025
NOTICE:  SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.12-v11.00.12 (Fancy Rat)')
ERROR:   Agent 0 Protocol 0x10 Message 0x7: not supportedU-Boot SPL 2025.01-00464-g1d6ba4a32cdd-dirty (May 29 2025 - 19:36:32 +0000)
 


Could you please guide me if I am missing any required changes ?

Best,
Parv