Part Number: AM6442
Hi Team,
We are trying to build industrial sdk(ind_comms_sdk_am64x_11_00_00_13) for ethercat_slave_beckhoff_ssc_demo for r5f1_0 booting via A53 linux kernel using remoteproc framework. With ethercat stacks added, we could able to generate am64-main-r5f1_0-fw file for r5f1_0 core and placing in /lib/firmware/mcubenchmarkdemo, and boot via a53 using echo cmd, faced error -22, With one of TI support thread assistance, I changed the memory mapping from MSRAM to DDR, and then I could see the linux prints as
[ 60.960808] remoteproc remoteproc2: powering up 78400000.r5f
[ 60.965177] remoteproc remoteproc2: Booting fw image am64-main-r5f1_0-fw, size 62868
[ 60.967636] remoteproc remoteproc2: remote processor 78400000.r5f is now up
added syscfg and linkercmd for your ref.
syscfg.txt.txt
linker_cmd.txt.txt
but from r5f fw, main is not executing in thread, on debugging it crashes in _c_int00 call from startup, can you provide solution on this.