This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: OSPI Slave mode support

Part Number: AM2431

Hi,

I would like you to confirm whether user can use OSPI of AM243X as slave mode or not.
I found following information for AM62.
AM623: OSPI Slave? - Processors forum - Processors - TI E2E support forums 
According to this, linux driver do not support slave mode for OSPI, but let me confirm whether this also can be applied to AM243X which R5 is main core or not.
Could you check about this ? 

Best Regards,

  • Hello,

    On the Sitara Processors and AM243, the OSPI is going to operate in Controller/Master mode and the driver is written in polling mode of operation.

    So currently, there is no support for OSPI acting as Peripheral/Slave.

    Regards,

    Vaibhav