This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2431: How extent does its temperature rise

Part Number: AM2431

Hi experts,

It is related to the following thread:AM2431: Why a substrate with Tg above 170 °C is used - Processors forum - Processors - TI E2E support forums 

My customer are considering AM2431.
Q: When using all its functions fully, to how extent does its temperature rise?

The maximum estimate Ta is 50 °C.
From the figure below, is it correct to calculate as: Max 1.9 [W] × 12.8 [R(Theta)JA (Junction-to-free air)] = +24.32 [Ta]?

Best regards,
O.H