Part Number: AM3357
I am encountering issues with IEEE 1588 PTP synchronization on a custom board based on the AM3357 processor. The system is configured with an external grandmaster clock acting as the PTP master, while the custom board operates as a PTP slave. All required kernel configurations and driver options for PTP support have been enabled. I have evaluated both hardware timestamping (MAC/PHY-based) and software timestamping modes; however, the slave node fails to achieve synchronization with the grandmaster clock in both cases.
This the .cfg file i'm using:

The following logs were captured during testing and are identical for both hardware and software timestamping modes.

Below is the settings of GrandMaster Clock:

I would appreciate TI’s technical support in helping me debug this issue and achieve proper PTP operation on the AM3357 platform.