This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM68A: H265 slice_parttioning_method

Part Number: AM68A

We are moving from h264 to h265 and focused on achieving as small latency as possible. Because of this we wanted to utilize slicing in h265. However, the only parameters I've seen are:

       number_of_mbs_in_a_slice 0x009909dc (int)    : min=0 max=65535 step=1 default=0 value=0
      slice_parttioning_method 0x009909dd (menu)   : min=0 max=1 default=0 value=0 (Single)
                0: Single
                1: Max Macroblocks

Considering, that it states macroblocks and not ctus, it looks like h265 is not supported. I've also tried to enable slice_parttioning_method=1 for v4l2h265enc, but it was just crashing.