Part Number: SK-AM62B-P1
Hi Team,
We have customized the board taking SK-AM62B-P1 as a reference and here are the schematics of the custom board.
optilink_1_build2_sch.pdf
We used GP SOC on the board, so we have used the default SD Image from 08.05 version and we have encountered this on Console when board is trying to Boot.
U-Boot SPL 2021.01-g3983bffabc (Dec 14 2022 - 11:53:21 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate t o prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate t o prevent boot failure. This will fail if the image was also encrypted
Loading Environment from MMC... *** Warning - No MMC card found, using default e nvironment
Starting ATF on ARM64 core...
NOTICE: BL31: v2.7(release):v2.7.0-359-g1309c6c805-dirty
NOTICE: BL31: Built : 11:48:12, Dec 14 2022
I/TC:
I/TC: OP-TEE version: 3.19.0-15-gd6c5d0037 (gcc version 9.2.1 20191025 (GNU Tool chain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Wed Dec 14 11:5 2:03 UTC 2022 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/ porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot
U-Boot SPL 2021.01-g3983bffabc (Dec 14 2022 - 11:52:19 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar')
Trying to boot from MMC2
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
spl: mmc init failed with error: -70
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
On discussion with below thread I made the chnages accrodingly and tried to make the SD Boot but there is no Console output when I have followed the Specified Steps.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1611523/sk-am62b-p1-am62x-custom-board-pmic-power-ok-sd-card-inserted-with-image-no-uart-or-peripheral-activity/6244811
On our Custom board we have unpopulated this one:
I have disabled the acknowledgemnt and tried to build bootloader files.
This has been seen on Console:
U-Boot SPL 2021.01-g3983bffabc (Dec 14 2022 - 11:53:21 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar')
SPL initial stack usage: 13424 bytes
Trying to boot from MMC2
Loading Environment from MMC... *** Warning - No MMC card found, using default environment
## No elf image at address 0x89000000
Starting ATF on ARM64 core...
NOTICE: BL31: v2.7(release):v2.7.0-359-g1309c6c805-dirty
NOTICE: BL31: Built : 11:48:12, Dec 14 2022
I/TC:
I/TC: OP-TEE version: 3.19.0-15-gd6c5d0037 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2014
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check optee.readthedocs.io/.../porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.5.3--v08.05.03 (Chill Capybar')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot
We are stuck at Board bring-Up and Need some infowith Custom Boot Loader generation.
Looking forward for assistance.
Regards,
Mallika