This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AH-Q1: Thermal Improvements

Part Number: TDA4AH-Q1
Other Parts Discussed in Thread: AM69

Hi Team

I created a new thread to proceed directly with the customer:

#################################################

I woould like to suggest to figure out what are the hardware and firmware settings for example for following configurations:

- 8x A72 1.5GHz

- 4x A72 1.5GHz

- 8x A72 1.0GHz

- 4x A72 1.0GHz

as i mentioned on this step of development for this poduct we can provide less performance, also set as a non changable configuration, only to reduce the power consumption, for the next performance level of the products where we can have bigger housing and maybe different type of cooling there we expect to have the full performance even with that high power consumption.

Do you think you could provide such hardware firmware configurations for us?

I think such type of documentation is not available?


Regards,

Fabio